HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
Core bias change timeout.
Steady state timeout duration for first lock.
Steady state timeout duration.
XO pin startup tuning capacitance.
XI pin startup tuning capacitance.
Core bias startup current.
Core bias intermediate startup current.
Core degeneration control.
Fixed tuning capacitance on XI/XO.
Tuning capacitance on XO.
Tuning capacitance on XI.
Core bias current.
Enable XI internal DC bias.
Oscillator mode.
Force XO pin to ground.
Force XI pin to ground.
Disable on-demand requests.
Force oscillator enable.
Lock register access.
Public Attribute Documentation#
timeoutCbLsb#
CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb
Core bias change timeout.
839
of file platform/emlib/inc/em_cmu.h
timeoutSteadyFirstLock#
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock
Steady state timeout duration for first lock.
840
of file platform/emlib/inc/em_cmu.h
timeoutSteady#
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady
Steady state timeout duration.
841
of file platform/emlib/inc/em_cmu.h
ctuneXoStartup#
uint8_t CMU_HFXOInit_TypeDef::ctuneXoStartup
XO pin startup tuning capacitance.
842
of file platform/emlib/inc/em_cmu.h
ctuneXiStartup#
uint8_t CMU_HFXOInit_TypeDef::ctuneXiStartup
XI pin startup tuning capacitance.
843
of file platform/emlib/inc/em_cmu.h
coreBiasStartup#
uint8_t CMU_HFXOInit_TypeDef::coreBiasStartup
Core bias startup current.
844
of file platform/emlib/inc/em_cmu.h
imCoreBiasStartup#
uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup
Core bias intermediate startup current.
845
of file platform/emlib/inc/em_cmu.h
coreDegenAna#
CMU_HfxoCoreDegen_TypeDef CMU_HFXOInit_TypeDef::coreDegenAna
Core degeneration control.
846
of file platform/emlib/inc/em_cmu.h
ctuneFixAna#
CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna
Fixed tuning capacitance on XI/XO.
847
of file platform/emlib/inc/em_cmu.h
ctuneXoAna#
uint8_t CMU_HFXOInit_TypeDef::ctuneXoAna
Tuning capacitance on XO.
848
of file platform/emlib/inc/em_cmu.h
ctuneXiAna#
uint8_t CMU_HFXOInit_TypeDef::ctuneXiAna
Tuning capacitance on XI.
849
of file platform/emlib/inc/em_cmu.h
coreBiasAna#
uint8_t CMU_HFXOInit_TypeDef::coreBiasAna
Core bias current.
850
of file platform/emlib/inc/em_cmu.h
enXiDcBiasAna#
bool CMU_HFXOInit_TypeDef::enXiDcBiasAna
Enable XI internal DC bias.
851
of file platform/emlib/inc/em_cmu.h
mode#
CMU_HfxoOscMode_TypeDef CMU_HFXOInit_TypeDef::mode
Oscillator mode.
852
of file platform/emlib/inc/em_cmu.h
forceXo2GndAna#
bool CMU_HFXOInit_TypeDef::forceXo2GndAna
Force XO pin to ground.
853
of file platform/emlib/inc/em_cmu.h
forceXi2GndAna#
bool CMU_HFXOInit_TypeDef::forceXi2GndAna
Force XI pin to ground.
854
of file platform/emlib/inc/em_cmu.h
disOnDemand#
bool CMU_HFXOInit_TypeDef::disOnDemand
Disable on-demand requests.
855
of file platform/emlib/inc/em_cmu.h
forceEn#
bool CMU_HFXOInit_TypeDef::forceEn
Force oscillator enable.
856
of file platform/emlib/inc/em_cmu.h
regLock#
bool CMU_HFXOInit_TypeDef::regLock
Lock register access.
860
of file platform/emlib/inc/em_cmu.h