IrDA Initialization structure.
Public Attributes#
General EUSART initialization structure.
bool
Enable the IrDA low frequency mode. Only RX operation are enabled.
Set to enable filter on IrDA demodulator.
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
Public Attribute Documentation#
init#
EUSART_UartInit_TypeDef EUSART_IrDAInit_TypeDef::init
General EUSART initialization structure.
Definition at line
502
of file platform/emlib/inc/em_eusart.h
irDALowFrequencyEnable#
bool EUSART_IrDAInit_TypeDef::irDALowFrequencyEnable
Enable the IrDA low frequency mode. Only RX operation are enabled.
Definition at line
505
of file platform/emlib/inc/em_eusart.h
irDARxFilterEnable#
EUSART_IrDARxFilterEnable_TypeDef EUSART_IrDAInit_TypeDef::irDARxFilterEnable
Set to enable filter on IrDA demodulator.
Definition at line
508
of file platform/emlib/inc/em_eusart.h
irDAPulseWidth#
EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
Definition at line
512
of file platform/emlib/inc/em_eusart.h