SE Command structure to which all commands to the SE must adhere.
Public Attributes#
uint32_t
SE Command.
Input data.
Output data.
uint32_t
Parameters.
size_t
Number of parameters.
Public Attribute Documentation#
command#
uint32_t SE_Command_t::command
SE Command.
Definition at line
146
of file platform/emlib/inc/em_se.h
data_in#
SE_DataTransfer_t* SE_Command_t::data_in
Input data.
Definition at line
147
of file platform/emlib/inc/em_se.h
data_out#
SE_DataTransfer_t* SE_Command_t::data_out
Output data.
Definition at line
148
of file platform/emlib/inc/em_se.h
parameters#
uint32_t SE_Command_t::parameters[SE_MAX_PARAMETERS]
Parameters.
Definition at line
149
of file platform/emlib/inc/em_se.h
num_parameters#
size_t SE_Command_t::num_parameters
Number of parameters.
Definition at line
150
of file platform/emlib/inc/em_se.h