Powersave Standby Associated#

Introduction#

This application demonstrates the process for configuring the RS9116W WiSeConnect EVK in power save profile mode 2.

It provides the steps to configure the RS9116W EVK in station mode and initiate a connection to an Access Point. When the module is in deep sleep, it wakes up in periodic intervals based on DTIM or Listen Interval.

If the UDP data transfer feature is enabled, the application then connects to a remote server to send UDP data in power save mode.

The application also enables the analysis of various power save profiles using a power analyzer during the Associated state with data transfer via UDP.

Setting Up#

To use this application, the following hardware, software and project setup is required.

Hardware Requirements#

Figure: Setup Diagram for Power Save Standby ExampleFigure: Setup Diagram for Power Save Standby Example

Software Requirements#

Application Build Environment#

The application can be configured to suit your requirements and development environment. Read through the following sections and make any changes needed.

Host Interface#

  • By default, the application is configured to use the SPI bus for interfacing between Host platforms(STM32F411 Nucleo / EFR32MG21) and the RS9116W EVK.

  • This application is also configured to use the SDIO bus for interfacing between Host platforms(EFM32GG11) and the RS9116W EVK.

Project Configuration#

The application is provided with the project folder consists of Keil and Simplicity Studio project files.

  • Keil project:

    • The Keil project can be executed on STM32 platform.

    • Project Path : <SDK>\examples\featured\powersave_standby_associated\projects\powersave_standby_associated-nucleo-f411re.uvprojx

  • Simplicity Studio :

    • The Simplicity Studio project is used for evaluating the application on the Silabs EFx32 platforms.

    • EFR32MG21 platform

      • Project Path :

        • If the Radio Board is BRD4180A or BRD4181A, then access the path <SDK>\examples\featured\powersave_standby_associated\projects\device_shadow_logging_stats\projects\powersave_standby_associated-brd4180a-mg21.slsproj

        • If the Radio Board is BRD4180B or BRD4181B, then access the path <SDK>\examples\featured\powersave_standby_associated\projects\device_shadow_logging_stats\projects\powersave_standby_associated-brd4180b-mg21.slsproj

    • EFM32GG11 platform

      • Project path:<SDK>/examples/featured/powersave_standby_associated/projects/powersave_standby_associated-brd2204a-gg11.slsproj

Bare Metal/RTOS Support#

To select a bare metal configuration, see Selecting bare metal.

Application Configuration Parameters#

Wi-Fi Configuration#

Configure the following parameters in rsi_wlan_connected_sleep_app.c to enable your Silicon Labs Wi-Fi device to connect to your Wi-Fi network.

#define SSID           "SILABS_AP"      // Wi-Fi Network Name
#define PSK            "1234567890"     // Wi-Fi Password
#define SECURITY_TYPE  RSI_WPA2         // Wi-Fi Security Type: RSI_OPEN / RSI_WPA / RSI_WPA2

Iperf Configuration#

  • SERVER_PORT is the remote UDP server port number on the PC running Iperf.

  • SERVER_IP_ADDRESS is the remote UDP server IP address on the PC running Iperf. IP address should be in long format and in little endian byte order Example: To configure "192.168.10.100" as the IP address, update the macro DEVICE_IP as 0x640AA8C0

  #define SERVER_PORT        <remote port>
  #define SERVER_IP_ADDRESS  0x640AA8C0      // 192.168.10.100 => | 0x64 = 100 | 0x0A = 10 | 0xA8 = 168 | 0xC0 = 192 |

Note! The feature to connect to a remote UDP server is disabled by default. To enable this feature, see common steps

Memory & Throughput#

  • NUMBER_OF_PACKETS controls the number of packets sent to the remote UDP server.

  • GLOBAL_BUFF_LEN sets the application memory size (in bytes) used by the driver.

  #define NUMBER_OF_PACKETS  <number of packets>
  #define GLOBAL_BUFF_LEN    15000

RTOS Options#

The following parameters are configured when FreeRTOS is used.

  #define RSI_WLAN_TASK_PRIORITY        1   // Should be low priority
  #define RSI_DRIVER_TASK_PRIORITY      2   // Should be highest priority 
  #define RSI_WLAN_TASK_STACK_SIZE    500   
  #define RSI_DRIVER_TASK_STACK_SIZE  500

Major Powersave Options#

The primary powersave settings are configured with PSP_MODE and PSP_TYPE. The default power save mode is set to low power mode 2 (RSI_SLEEP_MODE_2) with maximum power save (RSI_MAX_PSP) and with message based handshake as follows.

  #define PSP_MODE  RSI_SLEEP_MODE_2
  #define PSP_TYPE  RSI_MAX_PSP

PSP_MODE refers to the power save profile mode. RS9116W EVK supports the following power modes:

  • RSI_ACTIVE : In this mode, RS9116W EVK is active and power save is disabled.

  • RSI_SLEEP_MODE_1 : In this mode, RS9116W EVK goes to power save after association with the Access Point. In this sleep mode, SoC will never turn off, therefore no handshake is required before sending data to the RS9116W EVK.

  • RSI_SLEEP_MODE_2 : In this mode, RS9116W EVK goes to power save after association with the Access Point. In this sleep mode, SoC will go to sleep based on GPIO hand shake or Message exchange, therefore handshake is required before sending data to the RS9116W EVK.

  • RSI_SLEEP_MODE_8 : In this mode, RS9116W EVK goes to power save when it is not in associated state with the Access Point. In this sleep mode, SoC will go to sleep based on GPIO handshake or Message exchange, therefore handshake is required before sending the command to the RS9116W EVK.


Note!

  1. For RSI_SLEEP_MODE_2 and RSI_SLEEP_MODE_8 modes, GPIO or Message based handshake can be selected using RSI_HAND_SHAKE_TYPE macro which is defined in rsi_wlan_config.h.

  2. In this example, RSI_SLEEP_MODE_2 can be verified with a Message-based handshake. To verify other power modes, change the application as well as GPIO handshake signals.


PSP_TYPE refers to power save profile type. RS9116W EVK supports following power save profile types:

  • RSI_MAX_PSP : In this mode, RS9116W EVK will be in Maximum power save mode. i.e device will wake up for every DTIM beacon and do data Tx and Rx.

  • RSI_FAST_PSP : In this mode, RS9116W EVK will disable power save for any Tx/Rx packet for monitor interval of time (monitor interval can be set through macro in rsi_wlan_config.h file, default value is 50 ms). If there is no data for monitor interval of time, then RS9116W EVK will again enable power save.

  • RSI_UAPSD : This PSP_TYPE is used to enable WMM power save.


Note!

  1. PSP_TYPE is valid only when PSP_MODE is set to RSI_SLEEP_MODE_1 or RSI_SLEEP_MODE_2 mode.

  2. RSI_UAPSD power profile type in PSP_TYPE is valid only when RSI_WMM_PS_ENABLE is enabled in rsi_wlan_config.h file.


Additional Powersave Options#

Additional powersave options may be configured in rsi_wlan_config.h.

  #define CONCURRENT_MODE                     RSI_DISABLE
  #define RSI_FEATURE_BIT_MAP                 (FEAT_SECURITY_OPEN | FEAT_AGGREGATION | FEAT_ULP_GPIO_BASED_HANDSHAKE)
  #define RSI_TCP_IP_BYPASS                   RSI_DISABLE
  #define RSI_TCP_IP_FEATURE_BIT_MAP          (TCP_IP_FEAT_EXTENSION_VALID | TCP_IP_FEAT_DHCPV4_CLIENT)
  #define RSI_CUSTOM_FEATURE_BIT_MAP          FEAT_CUSTOM_FEAT_EXTENTION_VALID
  #define RSI_EXT_CUSTOM_FEATURE_BIT_MAP      (EXT_FEAT_LOW_POWER_MODE | EXT_FEAT_XTAL_CLK_ENABLE)
  #define RSI_EXT_TCPIP_FEATURE_BITMAP        CONFIG_FEAT_EXTENTION_VALID
  #define RSI_CONFIG_FEATURE_BITMAP           RSI_FEAT_SLEEP_GPIO_SEL_BITMAP
  #define RSI_BAND                            RSI_BAND_2P4GHZ
  
  The default configuration of low power_save_mode_2 is:
  
  #define RSI_HAND_SHAKE_TYPE                 GPIO_BASED
  #define RSI_SELECT_LP_OR_ULP_MODE           RSI_ULP_WITH_RAM_RET
  #define RSI_DTIM_ALIGNED_TYPE               0
  #define RSI_MONITOR_INTERVAL                50
  #define RSI_WMM_PS_ENABLE                   RSI_DISABLE
  #define RSI_WMM_PS_TYPE                     0
  #define RSI_WMM_PS_WAKE_INTERVAL            20
  #define RSI_WMM_PS_UAPSD_BITMAP             15

The application defaults to the RSI_SLEEP_MODE_2 configuration. Other powersave options are possible by choosing different powersave modes according to the following description.

  • RSI_HAND_SHAKE_TYPE is used to select the hand shake type (GPIO or Message) in RSI_SLEEP_MODE_2 and RSI_SLEEP_MODE_8 modes.

  • RSI_SELECT_LP_OR_ULP_MODE is used to select low power mode or ultra-low power mode. Valid configurations are

    • RSI_LP_MODE - RS9116W will be in Ultra low power mode.

    • RSI_ULP_WITH_RAM_RET - RS9116W will be in Ultra low power mode and will remember the previous state after issuing the power save mode command.

    • RSI_ULP_WITHOUT_RAM_RET - RS9116W will be in Ultra low power mode and it will not remember the previous state after issuing power save mode command. After wakeup, RS9116W will give CARD READY indication and user has to issue commands from wireless initialization.

  • RSI_DTIM_ALIGNED_TYPE is used to decide whether RS9116W has to wake up at normal beacon or DTIM beacon which is just before listen interval.

    • RSI_DTIM_ALIGNED_TYPE = 0 - RS9116W will wake up at normal beacon which is just before listen interval.

    • RSI_DTIM_ALIGNED_TYPE = 1 - RS9116W will wake up at DTIM beacon which is just before listen interval.

  • RSI_MONITOR_INTERVAL refers to the amount of time (in ms) to wait for Tx or Rx before giving power save indication to the connected Access Point. This macro is applicable only when PSP_TYPE selected as RSI_FAST_PSP

  • RSI_WMM_PS_ENABLE is used to enable or disable WMM power save.

  • RSI_WMM_PS_TYPE is used to set Tx-based or Periodic-based WMM power save. Set RSI_WMM_PS_TYPE = 0 for Tx based or =1 for periodic based WMM power save.

  • RSI_WMM_PS_WAKE_INTERVAL refers to the periodic time (in ms) in which the module has to wake up when RSI_WMM_PS_TYPE is selected as Periodic.

  • RSI_WMM_PS_UAPSD_BITMAP refers to the UAPSD bitmap. If RSI_WMM_PS_ENABLE is enabled, then PSP_TYPE must be set to RSI_UAPSD in order to WMM power save to work.

Testing the Application#

Follow the steps below for the successful execution of the application.

Loading the RS9116W Firmware#

Refer Getting started with a PC to load the firmware into RS9116W EVK.

The firmware file is located in <SDK>/firmware/

Building the Application on Host Platform#

Using STM32#

Refer Getting started with STM32

  • Connect STM32 CN10 header pin-4 to UULP_GPIO_0

  • Connect STM32 CN10 header pin-2 to UULP_GPIO_2

  • Open the project <SDK>\examples\featured\powersave_standby_associated\projects\powersave_standby_associated-nucleo-f411re.uvprojx

  • Build and debug the project.

  • Check for the RESET pin:

    • If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before Free run.

    • If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before Free run.

  • Free run the project.

  • Then continue the common steps.

Using EFx32#

Refer Getting started with EFx32, for settin-up EFR & EFM host platforms

  • Connect EFx32 J4 pin-9 to UULP_GPIO_0

  • Connect EFx32 J4 pin-7 to UULP_GPIO_2

  • Open Simplicity Studio and import the project <SDK>\examples\featured\powersave_standby_associated\projects

  • Select the appropriate .slsproj as per the Radio Board type mentioned in Project Configuration for Simplicity Studio.

  • Compile and flash the project in to Host MCU

  • Debug the project

  • Check for the RESET pin:

    • If RESET pin is connected from EFx32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run

    • If RESET pin is not connected from EFx32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run

  • Free run the project

  • Then continue the common steps.

Common Steps#

To enable the feature for data transfer with remote UDP server, follow the steps given below.

  • Open the project in Simplicity Studio

  • Right click on the project and choose 'Properties'

  • Go to 'C/C++ Build' | 'Settings' | 'GNU ARM C Compiler' | 'Preprocessor' and add the macro 'ENABLE_DATA_TRANSFER_DEMO=1'

  • Select 'Apply' and 'OK' to save the settings

With the feature now enabled, open a command prompt on the remote PC connected to the Wi-Fi access point. Start a UDP server using the below command in command prompt.

C:\ iperf.exe –s -u -p <SERVER_PORT> -i 1

Figure: command prompt on the remote PCFigure: command prompt on the remote PC

When the powersave application runs, RS9116W scans and connect to the Wi-Fi access point and obtains an IP address. After a successful connection, the device goes into configured power save and sends configured number of UDP packets to the remote peer which is connected to access point. The following image shows active reception of UDP data on the UDP server.

Figure: UDP packets to the remote peerFigure: UDP packets to the remote peer

Selecting Bare Metal#

The application has been designed to work with FreeRTOS and Bare Metal configurations. By default, the application project files (Keil and Simplicity studio) are configured with FreeRTOS enabled. The following steps demonstrate how to configure Simplicity Studio and Keil to test the application in a Bare Metal environment.

Bare Metal with Simplicity Studio#

  • Open the project in Simplicity Studio

  • Right click on the project and choose 'Properties'

  • Go to 'C/C++ Build' | 'Settings' | 'GNU ARM C Compiler' | 'Symbols' and remove macro 'RSI_WITH_OS=1'

  • Select 'Apply' and 'OK' to save the settings

Figure: project settings in Simplicity StudioFigure: project settings in Simplicity Studio

Figure: project settings in Simplicity StudioFigure: project settings in Simplicity Studio

Bare Metal with Keil#

  • Open the project in Keil and select 'Options for Target'

  • Go to the 'C/C++' tab and remove 'RSI_WITH_OS' macro present under Preprocessor Symbols

  • Select 'OK' to save the settings

Figure: project settings in Keil IDEFigure: project settings in Keil IDE

Compressed Debug Logging#

To enable the compressed debug logging feature please refer to Logging User Guide