Public Attribute Documentation#
status#
uint8_t status
Advertising Status
0 - disable
1 - enable
375
of file include/rsi_ble.h
adv_type#
uint8_t adv_type
Advertising type used during advertising
Advertising will be visible(discoverable) to all the devices. Scanning/Connection is also accepted from all devices.
#define UNDIR_CONN 0x80Advertising will be visible(discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only.
Scanning and Connection will be accepted from that device only.
#define DIR_CONN 0x81Advertising will be visible(discoverable) to all the devices. Scanning will be accepted from all the devices.
Connection will be not be accepted from any device.
#define UNDIR_SCAN 0x82Advertising will be visible(discoverable) to all the devices. Scanning and Connection will not be accepted from any device.
#define UNDIR_NON_CONN 0x83Advertising will be visible(discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only.
Scanning and Connection will be accepted from that device only.
#define DIR_CONN_LOW_DUTY_CYCLE 0x84
390
of file include/rsi_ble.h
filter_type#
uint8_t filter_type
Advertising filter type
#define ALLOW_SCAN_REQ_ANY_CONN_REQ_ANY 0x00
#define ALLOW_SCAN_REQ_ACCEPT_LIST_CONN_REQ_ANY 0x01
#define ALLOW_SCAN_REQ_ANY_CONN_REQ_ACCEPT_LIST 0x02
#define ALLOW_SCAN_REQ_ACCEPT_LIST_CONN_REQ_ACCEPT_LIST 0x03
396
of file include/rsi_ble.h
direct_addr_type#
uint8_t direct_addr_type
Address type of the device to which directed advertising has to be done
#define LE_PUBLIC_ADDRESS 0x00
#define LE_RANDOM_ADDRESS 0x01
#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02
#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
402
of file include/rsi_ble.h
direct_addr#
uint8_t direct_addr[RSI_DEV_ADDR_LEN]
Address of the device to which directed advertising has to be done
404
of file include/rsi_ble.h
adv_int_min#
uint16_t adv_int_min
Advertising interval min 0x0020 to 0x4000
407
of file include/rsi_ble.h
adv_int_max#
uint16_t adv_int_max
Advertising interval max 0x0020 to 0x4000
410
of file include/rsi_ble.h
own_addr_type#
uint8_t own_addr_type
Address of the local device.
#define LE_PUBLIC_ADDRESS 0x00
#define LE_RANDOM_ADDRESS 0x01
#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02
#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
417
of file include/rsi_ble.h
adv_channel_map#
uint8_t adv_channel_map
Advertising channel map.
#define RSI_BLE_ADV_CHANNEL_MAP 0x01 or 0x03 or 0x07
421
of file include/rsi_ble.h