Public Attributes#uint8_tlenuint8_tatt_valuePublic Attribute Documentation#len#uint8_t lenLength of attribute value Definition at line 640 of file include/rsi_ble_apis.hatt_value#uint8_t att_value[RSI_DEV_ATT_LEN]Attribute values list. Each attribute value is maximum of size 240, please refer RSI_DEV_ATT_LEN Macro Definition at line 643 of file include/rsi_ble_apis.h