Public Attribute Documentation#
maxtxoctets#
uint16_t maxtxoctets
maxtxoctets
Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
Definition at line
886
of file include/rsi_ble_apis.h
maxtxtime#
uint16_t maxtxtime
maxtxtime
Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
Definition at line
890
of file include/rsi_ble_apis.h
maxrxoctets#
uint16_t maxrxoctets
maxrxoctets
Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
Definition at line
894
of file include/rsi_ble_apis.h
maxrxtime#
uint16_t maxrxtime
maxrxtime
Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.
Definition at line
898
of file include/rsi_ble_apis.h