Public Attributes#

uint8_t
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[6]

remote device address


Definition at line 2359 of file include/rsi_bt_apis.h

scope#

uint8_t scope

Scope refers which List of folder items to be accessed at present
0 - Media_Player_List
1 - Virtual_File_System
2 - Search
3 - NowPlaying


Definition at line 2366 of file include/rsi_bt_apis.h

start_item#

uint16_t start_item

The offset within the listing of the item, which should be the first
returned item. The first element in the listing is at offset 0.


Definition at line 2370 of file include/rsi_bt_apis.h

end_item#

uint16_t end_item

The offset within the listing of the item which should be the final returned item.
If this is set to a value beyond what is available, the TG shall return items from the
provided Start Item index to the index of the final item.
If the End Item index is smaller than the Start Item index, the TG shall return an error.
If CT requests too many items, TG can respond with a sub-set of the requested items.


Definition at line 2377 of file include/rsi_bt_apis.h

attr_cnt#

uint8_t attr_cnt

Request the Attributes present on the attr_cnt value
0x00 - All attributes are requested.
0x01-0xFE - The following Attribute List contains this number of attributes.
0xFF - No attributes are requested.


Definition at line 2383 of file include/rsi_bt_apis.h