AR command structure.

Public Attribute Documentation#

opcode#

uint8_t opcode[2]

Definition at line 995 of file include/rsi_bt.h

ar_enable#

uint16_t ar_enable

Definition at line 996 of file include/rsi_bt.h

_3m_state_continuous_fail_threshold#

uint16_t _3m_state_continuous_fail_threshold

Definition at line 997 of file include/rsi_bt.h

_3m_state_absolute_fail_threshold#

uint16_t _3m_state_absolute_fail_threshold

Definition at line 998 of file include/rsi_bt.h

_3m_state_relative_fail_threshold#

uint16_t _3m_state_relative_fail_threshold

Definition at line 999 of file include/rsi_bt.h

_2m_state_pass_threshold#

uint16_t _2m_state_pass_threshold

Definition at line 1000 of file include/rsi_bt.h

_2m_state_continuous_pass_threshold#

uint16_t _2m_state_continuous_pass_threshold

Definition at line 1001 of file include/rsi_bt.h