Public Attribute Documentation#

rsi_sel_read_fds#

rsi_fd_set* rsi_sel_read_fds

Definition at line 593 of file include/rsi_wlan_non_rom.h

rsi_sel_write_fds#

rsi_fd_set* rsi_sel_write_fds

Definition at line 596 of file include/rsi_wlan_non_rom.h

rsi_sel_exception_fds#

rsi_fd_set* rsi_sel_exception_fds

Definition at line 599 of file include/rsi_wlan_non_rom.h

rsi_sel_read_fds_var#

rsi_fd_set rsi_sel_read_fds_var

Definition at line 602 of file include/rsi_wlan_non_rom.h

rsi_sel_write_fds_var#

rsi_fd_set rsi_sel_write_fds_var

Definition at line 605 of file include/rsi_wlan_non_rom.h

rsi_sel_exception_fds_var#

rsi_fd_set rsi_sel_exception_fds_var

Definition at line 608 of file include/rsi_wlan_non_rom.h

select_sem#

rsi_semaphore_handle_t select_sem

Definition at line 611 of file include/rsi_wlan_non_rom.h

select_status#

int32_t select_status

Definition at line 613 of file include/rsi_wlan_non_rom.h

select_state#

uint8_t select_state

Definition at line 615 of file include/rsi_wlan_non_rom.h

select_id#

uint8_t select_id

Definition at line 617 of file include/rsi_wlan_non_rom.h

sock_select_callback#

void(* sock_select_callback) (rsi_fd_set *fd_read, rsi_fd_set *fd_write, rsi_fd_set *fd_except, int32_t status)

Definition at line 619 of file include/rsi_wlan_non_rom.h