Public Attributes#
Public Attribute Documentation#
numofitems#
uint16_t numofitems
Number of items present in that Folder
3522
of file include/rsi_bt_apis.h
itemtype#
uint8_t itemtype
Item_Type
1 - Media Player Item
2 - Folder Item
3 - Media Element Item
Note
But this structure is declared for Media_Player_Item
3529
of file include/rsi_bt_apis.h
playerid#
uint16_t playerid
A unique identifier for this media player.
3535
of file include/rsi_bt_apis.h
majorplayertype#
uint8_t majorplayertype
There are currently four base types of media player
BIT(0) - AUDIO_PLAYER (Eg: Mp3 Player)
BIT(1) - VIDEO_PLAYER (Eg: Mpeg4 Player)
BIT(2) - BROADCASTING_AUDIO (Eg: FM Radio)
BIT(3) - BROADCASTING_VIDEO (Eg: DVB-H Tuner)
3542
of file include/rsi_bt_apis.h
playersubtype#
uint32_t playersubtype
There are Two defined SubTypes
BIT(0) - AUDIO_BOOK
BIT(1) - PODCAST
3547
of file include/rsi_bt_apis.h
playstatus#
uint8_t playstatus
Current Play Status
0 - STOPPED
1 - PLAYING
2 - PAUSED
3 - FWD_SEEK
4 - REV_SEEK
FF - ERROR
3556
of file include/rsi_bt_apis.h
featurebitmask#
uint8_t featurebitmask[16]
Each Player on a TG announces its features to the CT in the PlayerFeatureBitmask
3559
of file include/rsi_bt_apis.h
charsetid#
uint16_t charsetid
Specifies the character set ID to be displayed on CT
3562
of file include/rsi_bt_apis.h
disnamelen#
uint16_t disnamelen
Length of Displayable Name. The name length shall be limited such that a response
to a GetFolderItems containing one media player item fits within the maximum size of
AVRCP PDU which can be received by the CT.
3567
of file include/rsi_bt_apis.h
disname#
uint8_t disname[11]
Displayable name of player
3570
of file include/rsi_bt_apis.h