Firmware up request structure.

Public Attributes#

uint16_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t

Public Attribute Documentation#

control_flags#

uint16_t control_flags

Definition at line 901 of file include/rsi_common.h

sha_type#

uint16_t sha_type

Definition at line 902 of file include/rsi_common.h

magic_no#

uint32_t magic_no

Definition at line 903 of file include/rsi_common.h

image_size#

uint32_t image_size

Definition at line 904 of file include/rsi_common.h

fw_version#

uint32_t fw_version

Definition at line 905 of file include/rsi_common.h

image_loc#

uint32_t image_loc

Definition at line 906 of file include/rsi_common.h

crc#

uint32_t crc

Definition at line 907 of file include/rsi_common.h