Public Attributes#

uint32_t
uint32_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

player_status#

uint8_t player_status

Play Status
0 - STOPPED
1 - PLAYING
2 - PAUSED
3 - FWD_SEEK
4 - REV_SEEK
FF - ERROR


Definition at line 1973 of file include/rsi_bt_apis.h

track_num#

uint32_t track_num

Current Playing Track Index


Definition at line 1976 of file include/rsi_bt_apis.h

track_pos#

uint32_t track_pos

Current playback position in millisecond


Definition at line 1979 of file include/rsi_bt_apis.h

battery_status#

uint8_t battery_status

Battery Status
0 - NORMAL
1 - WARNING
2 - CRITICAL
3 - EXTERNAL
4 - FULLCHARGE


Definition at line 1987 of file include/rsi_bt_apis.h

system_status#

uint8_t system_status

System Status
0 - POWER_ON
1 - POWER_OFF
2 - UNPLUGGED


Definition at line 1993 of file include/rsi_bt_apis.h

abs_vol#

uint8_t abs_vol

Absolute Volume Value


Definition at line 1996 of file include/rsi_bt_apis.h

playerid#

uint16_t playerid

Media Player ID


Definition at line 1999 of file include/rsi_bt_apis.h

uidcounter#

uint16_t uidcounter

Unique ID for the MediaPlayer


Definition at line 2002 of file include/rsi_bt_apis.h

att_val_list#

att_val_list_t att_val_list

Please refer att_val_list_s structure for more info


Definition at line 2005 of file include/rsi_bt_apis.h