Public Attribute Documentation#
dev_addr_type#
uint8_t dev_addr_type
Device address type of the Connected Remote Device
Definition at line
90
of file include/rsi_ble_apis.h
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
Device address of the remote device.
Definition at line
92
of file include/rsi_ble_apis.h
local_resolvlable_addr#
uint8_t local_resolvlable_addr[RSI_DEV_ADDR_LEN]
Local Device resolvable address
Definition at line
94
of file include/rsi_ble_apis.h
peer_resolvlable_addr#
uint8_t peer_resolvlable_addr[RSI_DEV_ADDR_LEN]
Remote Device resolvable address
Definition at line
96
of file include/rsi_ble_apis.h
role#
uint8_t role
The role of the device - master/ slave
Definition at line
98
of file include/rsi_ble_apis.h
conn_interval#
uint16_t conn_interval
Connection interval used on this connection. Range: 0x0006 to 0x0C80
Definition at line
100
of file include/rsi_ble_apis.h
conn_latency#
uint16_t conn_latency
Slave latency for the connection in number of connection events. Range: 0x0000 to 0x01F3
Definition at line
102
of file include/rsi_ble_apis.h
supervision_timeout#
uint16_t supervision_timeout
Connection supervision timeout. Range: 0x000A to 0x0C80
Definition at line
104
of file include/rsi_ble_apis.h
master_clock_accuracy#
uint8_t master_clock_accuracy
Only applicable for slave ,for master this value is set to 0x00
Definition at line
106
of file include/rsi_ble_apis.h
status#
uint8_t status
Status of the Connection - success/failure
Definition at line
108
of file include/rsi_ble_apis.h