Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
remote device address
Definition at line
706
of file include/rsi_ble_apis.h
offset#
uint8_t offset[2]
attribute value offset
Definition at line
710
of file include/rsi_ble_apis.h
length#
uint16_t length
length of attribute value
Definition at line
712
of file include/rsi_ble_apis.h
att_value#
uint8_t att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro
Definition at line
714
of file include/rsi_ble_apis.h