Public Attributes#

uint32_t

Public Attribute Documentation#

fail_count_3m#

uint32_t fail_count_3m

3m TX Fail Count


Definition at line 584 of file include/rsi_bt_apis.h

fail_count_2m#

uint32_t fail_count_2m

2m TX Fail Count


Definition at line 587 of file include/rsi_bt_apis.h

pass_count_3m#

uint32_t pass_count_3m

3m TX Pass Count


Definition at line 590 of file include/rsi_bt_apis.h

pass_count_2m#

uint32_t pass_count_2m

2m TX Pass Count


Definition at line 593 of file include/rsi_bt_apis.h

reason_code#

uint32_t reason_code

#define _3M_STATE_CONTINUOUS_FAIL_THRESHOLD_REACHED 1
#define _3M_STATE_PER_THRESHOLD_REACHED 2
#define _2M_STATE_PASS_THRESHOLD_REACHED 3
#define _2M_STATE_CONTINUOUS_PASS_THRESHOLD_REACHED 4
#define _BT_AR_STATS_PERIODIC 5


Definition at line 600 of file include/rsi_bt_apis.h

current_state#

uint32_t current_state

Current data rate state
#define STATE_3M_RATE BIT(0)
#define STATE_2M_RATE BIT(1)


Definition at line 605 of file include/rsi_bt_apis.h