Public Attributes#
Public Attribute Documentation#
dm1_pkt#
uint16_t dm1_pkt[2]
dm1_pkt[0] - Num of TXed dm1 Pkts
dm1_pkt[1] - Num of RXed dm1 Pkts
491
of file include/rsi_bt_apis.h
dm3_pkt#
uint16_t dm3_pkt[2]
dm3_pkt[0] - Num of TXed dm3 Pkts
dm3_pkt[1] - Num of RXed dm3 Pkts
495
of file include/rsi_bt_apis.h
dm5_pkt#
uint16_t dm5_pkt[2]
dm5_pkt[0] - Num of TXed dm5 Pkts
dm5_pkt[1] - Num of RXed dm5 Pkts
499
of file include/rsi_bt_apis.h
dh1_pkt#
uint16_t dh1_pkt[2]
dh1_pkt[0] - Num of TXed dh1 Pkts
dh1_pkt[1] - Num of RXed dh1 Pkts
503
of file include/rsi_bt_apis.h
dh3_pkt#
uint16_t dh3_pkt[2]
dh3_pkt[0] - Num of TXed dh3 Pkts
dh3_pkt[1] - Num of RXed dh3 Pkts
507
of file include/rsi_bt_apis.h
dh5_pkt#
uint16_t dh5_pkt[2]
dh5_pkt[0] - Num of TXed dh5 Pkts
dh5_pkt[1] - Num of RXed dh5 Pkts
511
of file include/rsi_bt_apis.h
edr_2dh1_pkt#
uint16_t edr_2dh1_pkt[2]
2dh1_pkt[0] - Num of TXed 2dh1 Pkts
2dh1_pkt[1] - Num of RXed 2dh1 Pkts
516
of file include/rsi_bt_apis.h
edr_2dh3_pkt#
uint16_t edr_2dh3_pkt[2]
2dh3_pkt[0] - Num of TXed 2dh3 Pkts
2dh3_pkt[1] - Num of RXed 2dh3 Pkts
520
of file include/rsi_bt_apis.h
edr_2dh5_pkt#
uint16_t edr_2dh5_pkt[2]
2dh5_pkt[0] - Num of TXed 2dh5 Pkts
2dh5_pkt[1] - Num of RXed 2dh5 Pkts
524
of file include/rsi_bt_apis.h
edr_3dh1_pkt#
uint16_t edr_3dh1_pkt[2]
3dh1_pkt[0] - Num of TXed 3dh1 Pkts
3dh1_pkt[1] - Num of RXed 3dh1 Pkts
528
of file include/rsi_bt_apis.h
edr_3dh3_pkt#
uint16_t edr_3dh3_pkt[2]
3dh3_pkt[0] - Num of TXed 3dh3 Pkts
3dh3_pkt[1] - Num of RXed 3dh3 Pkts
532
of file include/rsi_bt_apis.h
edr_3dh5_pkt#
uint16_t edr_3dh5_pkt[2]
3dh5_pkt[0] - Num of TXed 3dh5 Pkts
3dh5_pkt[1] - Num of RXed 3dh5 Pkts
536
of file include/rsi_bt_apis.h
no_of_crc_fail#
uint16_t no_of_crc_fail
Num of CRC Failed Packets
540
of file include/rsi_bt_apis.h
no_of_retries#
uint16_t no_of_retries
Num of Retransmission Packets
543
of file include/rsi_bt_apis.h
no_of_hdr_err#
uint16_t no_of_hdr_err
Num of Header Error Packets
546
of file include/rsi_bt_apis.h
no_of_seq_repeat#
uint16_t no_of_seq_repeat
Num of Duplicate Packets Received
(If previous sequence number is received again)
550
of file include/rsi_bt_apis.h
ack_delay#
uint16_t ack_delay[11]
Num of ack packets received with delay of 10ms to 100ms and more that 100ms
10 - ack_delay[10] ......... >100 - ack_delay[10]
554
of file include/rsi_bt_apis.h
ack_received#
uint16_t ack_received
Num of ACK packets Received
557
of file include/rsi_bt_apis.h
nak_received#
uint16_t nak_received
Num of NAK packets Received
560
of file include/rsi_bt_apis.h
no_of_rx_missed#
uint16_t no_of_rx_missed
Num of missed response packets in the RX Slot
563
of file include/rsi_bt_apis.h
no_of_rx_error#
uint16_t no_of_rx_error
Num of RXed error packets in the RX Slot
566
of file include/rsi_bt_apis.h
tx_attempts#
uint16_t tx_attempts
Num of TX Attempts
569
of file include/rsi_bt_apis.h
tx_done#
uint16_t tx_done
Number of Packets TXed on Air
572
of file include/rsi_bt_apis.h