Public Attributes#rsi_mutex_handle_tfw_log_pool_mutexFirmware log mutex. uint16_tsizePool total node count. uint16_tavailPool available node count. void **poolPool pointer. Public Attribute Documentation#fw_log_pool_mutex#rsi_mutex_handle_t fw_log_pool_mutexFirmware log mutex. Definition at line 33 of file include/sl_fw_logging.hsize#uint16_t sizePool total node count. Definition at line 35 of file include/sl_fw_logging.havail#uint16_t availPool available node count. Definition at line 37 of file include/sl_fw_logging.hpool#void** poolPool pointer. Definition at line 39 of file include/sl_fw_logging.h