Public Attributes#
uint32_t
uint32_t
rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
int32_t
uint8_t
int32_t
uint8_t
uint8_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint8_t
uint32_t
timer flag
rsi_device_state_t
uint8_t *
uint32_t
uint8_t
uint8_t
Public Attribute Documentation#
tx_mask_event#
uint32_t tx_mask_event
Definition at line
817
of file include/rsi_common.h
Referenced by rsi_tx_event_handler , and rsi_rx_event_handler
debug_prints_mutex#
rsi_mutex_handle_t debug_prints_mutex
Definition at line
823
of file include/rsi_common.h
nwk_sem#
rsi_semaphore_handle_t nwk_sem
Definition at line
825
of file include/rsi_common.h
Referenced by rsi_driver_deinit , and rsi_post_waiting_nwk_semaphore
wlan_cmd_sem#
rsi_semaphore_handle_t wlan_cmd_sem
Definition at line
826
of file include/rsi_common.h
Referenced by rsi_wireless_init , rsi_driver_deinit , rsi_post_waiting_wlan_semaphore , rsi_wlan_scan_with_bitmap_options , rsi_wlan_scan , and rsi_wlan_connect
common_cmd_sem#
rsi_semaphore_handle_t common_cmd_sem
Definition at line
827
of file include/rsi_common.h
Referenced by rsi_bt_callbacks_handler , and rsi_driver_deinit
common_cmd_send_sem#
rsi_semaphore_handle_t common_cmd_send_sem
Definition at line
828
of file include/rsi_common.h
wlan_cmd_send_sem#
rsi_semaphore_handle_t wlan_cmd_send_sem
Definition at line
829
of file include/rsi_common.h
Referenced by rsi_driver_deinit , and rsi_post_waiting_wlan_semaphore
nwk_cmd_send_sem#
rsi_semaphore_handle_t nwk_cmd_send_sem
Definition at line
830
of file include/rsi_common.h
Referenced by rsi_driver_deinit , and rsi_post_waiting_nwk_semaphore
send_data_sem#
rsi_semaphore_handle_t send_data_sem
Definition at line
831
of file include/rsi_common.h
nwk_wait_bitmap#
uint8_t nwk_wait_bitmap
Definition at line
832
of file include/rsi_common.h
Referenced by rsi_check_waiting_cmds , and rsi_post_waiting_nwk_semaphore
common_wait_bitmap#
uint8_t common_wait_bitmap
Definition at line
835
of file include/rsi_common.h
Referenced by rsi_bt_callbacks_handler , rsi_req_wakeup , rsi_check_waiting_cmds , and rsi_wireless_init
bt_cmd_wait_bitmap#
uint8_t bt_cmd_wait_bitmap
Definition at line
838
of file include/rsi_common.h
Referenced by rsi_bt_clear_wait_bitmap , and rsi_bt_set_wait_bitmap
common_cmd_state#
volatile uint8_t common_cmd_state
Definition at line
844
of file include/rsi_common.h
driver_timer_start#
volatile uint32_t driver_timer_start
Definition at line
847
of file include/rsi_common.h
driver_rx_timer_start#
volatile uint32_t driver_rx_timer_start
Definition at line
851
of file include/rsi_common.h
rx_timer_start#
rsi_timer_instance_t rx_timer_start
Definition at line
852
of file include/rsi_common.h
sdio_read_buff#
uint8_t sdio_read_buff[SDIO_BUFFER_LENGTH]
Definition at line
865
of file include/rsi_common.h
rx_driver_flag#
uint32_t rx_driver_flag
timer flag
Definition at line
868
of file include/rsi_common.h
device_state#
volatile rsi_device_state_t device_state
Definition at line
869
of file include/rsi_common.h
rsi_wait_timeout_handler_error_cb#
void(* rsi_wait_timeout_handler_error_cb) (int32_t status, uint32_t cmd_type)
Definition at line
872
of file include/rsi_common.h
Referenced by rsi_register_wait_timeout_error_callbacks , and rsi_wait_on_socket_semaphore
nwk_app_buffer_length#
uint32_t nwk_app_buffer_length
Definition at line
878
of file include/rsi_common.h