Public Attribute Documentation#

rsi_driver_cb#

struct rsi_driver_cb_s* rsi_driver_cb

Definition at line 121 of file include/rsi_apis_rom.h

rsi_socket_pool#

struct rsi_socket_info_s* rsi_socket_pool

Definition at line 124 of file include/rsi_apis_rom.h

rom_apis_p#

rom_apis_t* rom_apis_p

Definition at line 126 of file include/rsi_apis_rom.h

no_of_sockets#

uint8_t no_of_sockets

Definition at line 128 of file include/rsi_apis_rom.h

endian#

uint8_t endian

Definition at line 130 of file include/rsi_apis_rom.h

rx_buffer_mem_copy#

uint8_t rx_buffer_mem_copy

Definition at line 132 of file include/rsi_apis_rom.h

rsi_tcp_listen_min_backlog#

uint8_t rsi_tcp_listen_min_backlog

Definition at line 134 of file include/rsi_apis_rom.h

os_enabled#

uint8_t os_enabled

Definition at line 136 of file include/rsi_apis_rom.h

rsi_max_num_events#

uint8_t rsi_max_num_events

Definition at line 138 of file include/rsi_apis_rom.h

tx_desc#

struct rsi_m4ta_desc_s* tx_desc

Definition at line 140 of file include/rsi_apis_rom.h

rx_desc#

struct rsi_m4ta_desc_s* rx_desc

Definition at line 142 of file include/rsi_apis_rom.h

submit_rx_pkt_to_ta#

volatile uint8_t submit_rx_pkt_to_ta

Definition at line 144 of file include/rsi_apis_rom.h