Crypto APIs#
This section describes the Crypto APIs
Functions#
Compute the SHA digest. This is a blocking API.
Decide whether the SHA message can be sent once or requires multiple calls to send. This is a blocking API.
Hold computed digest from HMAC-SHA. This is a blocking API.
Decide whether the HMAC-SHA message can be sent once or requires multiple calls to send the message. This is a blocking API.
Decide whether the AES message can be sent once or requires multiple calls to send the message. This is a blocking API.
Calculate the DH key. This is a blocking API.
Compute the ECDH point multiplication vector. This is a blocking API.
Compute the ECDH point addition vector. This is a blocking API.
Compute the ECDH point subtraction vector. This is a blocking API.
Compute the ECDH point double vector. This is a blocking API.
Compute the ECDH point affinity vector. This is a blocking API.
Function Documentation#
rsi_sha_pen#
int32_t rsi_sha_pen (uint8_t sha_mode, uint8_t * msg, uint16_t msg_length, uint16_t chunk_len, uint8_t pending_flag, uint8_t * digest)
Compute the SHA digest. This is a blocking API.
[in] | sha_mode | 1 – For SHA1 |
[in] | msg | - Pointer to message |
[in] | msg_length | - Total message length |
[in] | chunk_len | - Current chunk length |
[in] | pending_flag | - BIT(0) - 1st chunk |
[out] | digest | - Output parameter to hold computed digest from SHA |
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer to Error Codes for the description of above error codes.
40
of file crypto/rsi_crypto.c
rsi_sha#
int32_t rsi_sha (uint8_t sha_mode, uint8_t * msg, uint16_t msg_length, uint8_t * digest)
Decide whether the SHA message can be sent once or requires multiple calls to send. This is a blocking API.
[in] | sha_mode | 1 – For SHA1 |
[in] | msg | - Pointer to message |
[in] | msg_length | - Total message length |
[out] | digest | - Output parameter to hold computed digest from SHA |
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer to Error Codes for the description of above error codes.
192
of file crypto/rsi_crypto.c
rsi_hmac_sha_pen#
int32_t rsi_hmac_sha_pen (uint8_t hmac_sha_mode, uint8_t * data, uint16_t total_length, uint16_t chunk_length, uint32_t key_length, uint8_t pending_flag, uint8_t * digest)
Hold computed digest from HMAC-SHA. This is a blocking API.
[in] | hmac_sha_mode | - 1 – For HMAC-SHA1 |
[in] | data | - Pointer to key along with message |
[in] | total_length | - Total message length |
[in] | chunk_length | - Current chunk length |
[in] | key_length | - BIT(0) - 1st chunk |
[out] | pending_flag | - Output parameter to hold computed digest from HMAC-SHA |
N/A | digest |
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer to Error Codes for the description of above error codes.
260
of file crypto/rsi_crypto.c
rsi_hmac_sha#
int32_t rsi_hmac_sha (uint8_t hmac_sha_mode, uint8_t * msg, uint32_t msg_length, uint8_t * key, uint32_t key_length, uint8_t * digest, uint8_t * hmac_buffer)
Decide whether the HMAC-SHA message can be sent once or requires multiple calls to send the message. This is a blocking API.
[in] | hmac_sha_mode | - 1 – For HMAC-SHA1 |
[in] | msg | - Pointer to message |
[in] | msg_length | - Total message length |
[in] | key | - Pointer to HMAC key |
[in] | key_length | - HMAC key length in bytes |
[out] | digest | - Output parameter to hold computed digest from HMAC-SHA |
N/A | hmac_buffer |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
422
of file crypto/rsi_crypto.c
rsi_aes#
int32_t rsi_aes (uint16_t aes_mode, uint16_t enc_dec, uint8_t * msg, uint16_t msg_length, uint8_t * key, uint16_t key_length, uint8_t * iv, uint8_t * output)
Decide whether the AES message can be sent once or requires multiple calls to send the message. This is a blocking API.
[in] | aes_mode | - 1 – For AES CBC mode |
[in] | enc_dec | - 1 – For AES Encryption |
[in] | msg | - Pointer to message |
[in] | msg_length | - Total message length |
[in] | key | - Pointer to AES key |
[in] | key_length | - AES key length in bytes |
[in] | iv | - Pointer to AES iv |
[out] | output | - Output parameter to hold encrypted/decrypted from AES |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
513
of file crypto/rsi_crypto.c
rsi_exponentiation#
int32_t rsi_exponentiation (uint8_t * prime, uint32_t prime_length, uint8_t * base, uint32_t base_length, uint8_t * exponent, uint32_t exponent_length, uint8_t * exp_result)
Calculate the DH key. This is a blocking API.
[in] | prime | - Pointer to the prime |
[in] | prime_length | - Length of the prime |
[in] | base | - Pointer to base |
[in] | base_length | - Length of the base |
[in] | exponent | - Pointer to exponent |
[in] | exponent_length | - Length of the exponent |
[out] | exp_result | - Output exponentiation result |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
759
of file crypto/rsi_crypto.c
rsi_ecdh_point_multiplication#
int32_t rsi_ecdh_point_multiplication (uint8_t ecdh_mode, uint8_t * d, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point multiplication vector. This is a blocking API.
[in] | ecdh_mode | - 1 – For ECDH 192 |
[in] | d | - Pointer to scalar value that needs to be multiplied |
[in] | sx | - Pointers to x, y, z coordinates of the point to be multiplied with scalar ‘d’ |
[out] | sy | - Pointers to x, y, z coordinates of the result point |
N/A | sz | |
N/A | rx | |
N/A | ry | |
N/A | rz |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
910
of file crypto/rsi_crypto.c
rsi_ecdh_point_addition#
int32_t rsi_ecdh_point_addition (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * tx, uint8_t * ty, uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point addition vector. This is a blocking API.
[in] | ecdh_mode | - 1 – For ECDH 192 |
[in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be added |
[in] | sy | - Pointers to x, y, z coordinates of the point2 that needs to be added |
[out] | sz | - Pointers to x, y, z coordinates of the result point |
N/A | tx | |
N/A | ty | |
N/A | tz | |
N/A | rx | |
N/A | ry | |
N/A | rz |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
1077
of file crypto/rsi_crypto.c
rsi_ecdh_point_subtraction#
int32_t rsi_ecdh_point_subtraction (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * tx, uint8_t * ty, uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point subtraction vector. This is a blocking API.
[in] | ecdh_mode | - 1 – For ECDH 192 |
[in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be subtracted |
[in] | sy | - Pointers to x, y, z coordinates of the point2 that needs to be subtracted |
[out] | sz | - Pointers to x, y, z coordinates of the result point |
N/A | tx | |
N/A | ty | |
N/A | tz | |
N/A | rx | |
N/A | ry | |
N/A | rz |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
1256
of file crypto/rsi_crypto.c
rsi_ecdh_point_double#
int32_t rsi_ecdh_point_double (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point double vector. This is a blocking API.
[in] | ecdh_mode | - 1 – For ECDH 192 |
[in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be doubled |
[out] | sy | - Pointers to x, y, z coordinates of the result point |
N/A | sz | |
N/A | rx | |
N/A | ry | |
N/A | rz |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
1438
of file crypto/rsi_crypto.c
rsi_ecdh_point_affine#
int32_t rsi_ecdh_point_affine (uint8_t ecdh_mode, uint8_t * sx, uint8_t * sy, uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
Compute the ECDH point affinity vector. This is a blocking API.
[in] | ecdh_mode | - 1 – For ECDH 192 |
[in] | sx | - Pointers to x, y, z coordinates of the point1 that needs to be affinified |
[out] | sy | - Pointers to x, y, z coordinates of the result point |
N/A | sz | |
N/A | rx | |
N/A | ry | |
N/A | rz |
Returns
0 - Success
Non-Zero Value - Failure (Possible Error Codes - 0xfffffffe, 0xfffffffd, 0xfffffffc, 0xFF15, 0xCC9C, 0xCC9B)
Note
Refer to Error Codes for the description of above error codes.
1597
of file crypto/rsi_crypto.c