Public Attribute Documentation#

eap_profile_magic_word#

uint8_t eap_profile_magic_word[4]

Definition at line 1210 of file include/rsi_wlan_apis.h

wlan_feature_bit_map#

uint8_t wlan_feature_bit_map[4]

Definition at line 1211 of file include/rsi_wlan_apis.h

tcp_ip_feature_bit_map#

uint8_t tcp_ip_feature_bit_map[4]

Definition at line 1212 of file include/rsi_wlan_apis.h

custom_feature_bit_map#

uint8_t custom_feature_bit_map[4]

Definition at line 1213 of file include/rsi_wlan_apis.h

listen_interval#

uint8_t listen_interval

Definition at line 1214 of file include/rsi_wlan_apis.h

data_rate#

uint8_t data_rate

Definition at line 1215 of file include/rsi_wlan_apis.h

tx_power#

uint8_t tx_power

Definition at line 1216 of file include/rsi_wlan_apis.h

band#

uint8_t band

Definition at line 1217 of file include/rsi_wlan_apis.h

ssid#

uint8_t ssid[RSI_SSID_LEN]

Definition at line 1218 of file include/rsi_wlan_apis.h

ssid_len#

uint8_t ssid_len

Definition at line 1219 of file include/rsi_wlan_apis.h

channel#

uint8_t channel[2]

Definition at line 1220 of file include/rsi_wlan_apis.h

scan_feature_bitmap#

uint8_t scan_feature_bitmap

Definition at line 1221 of file include/rsi_wlan_apis.h

scan_chan_bitmap_magic_code#

uint8_t scan_chan_bitmap_magic_code[2]

Definition at line 1222 of file include/rsi_wlan_apis.h

scan_chan_bitmap_2_4_ghz#

uint8_t scan_chan_bitmap_2_4_ghz[4]

Definition at line 1223 of file include/rsi_wlan_apis.h

scan_chan_bitmap_5_0_ghz#

uint8_t scan_chan_bitmap_5_0_ghz[4]

Definition at line 1224 of file include/rsi_wlan_apis.h

security_type#

uint8_t security_type

Definition at line 1225 of file include/rsi_wlan_apis.h

eap_method#

uint8_t eap_method[32]

Definition at line 1226 of file include/rsi_wlan_apis.h

inner_method#

uint8_t inner_method[32]

Definition at line 1227 of file include/rsi_wlan_apis.h

user_identity#

uint8_t user_identity[64]

Definition at line 1228 of file include/rsi_wlan_apis.h

passwd#

uint8_t passwd[128]

Definition at line 1229 of file include/rsi_wlan_apis.h

network_profile#

network_profile_t network_profile

Definition at line 1232 of file include/rsi_wlan_apis.h

feature_frame_params_s#

feature_frame_params_t feature_frame_params_s

Definition at line 1233 of file include/rsi_wlan_apis.h