Struct wrapper for all data for a command which comes in over the air. This enables struct is used to encapsulate a command in a single place on the stack and pass a pointer to that location around during command processing.
Public Attributes#
EmberApsFrame *
EmberIncomingMessageType
EmberNodeId
uint8_t *
uint16_t
bool
bool
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
Public Attribute Documentation#
apsFrame#
EmberApsFrame* EmberAfClusterCommand::apsFrame
APS frame for the incoming message
Definition at line
432
of file app/framework/include/af-types.h
type#
EmberIncomingMessageType EmberAfClusterCommand::type
Definition at line
433
of file app/framework/include/af-types.h
source#
EmberNodeId EmberAfClusterCommand::source
Definition at line
434
of file app/framework/include/af-types.h
buffer#
uint8_t* EmberAfClusterCommand::buffer
Definition at line
435
of file app/framework/include/af-types.h
bufLen#
uint16_t EmberAfClusterCommand::bufLen
Definition at line
436
of file app/framework/include/af-types.h
clusterSpecific#
bool EmberAfClusterCommand::clusterSpecific
Definition at line
437
of file app/framework/include/af-types.h
mfgSpecific#
bool EmberAfClusterCommand::mfgSpecific
Definition at line
438
of file app/framework/include/af-types.h
mfgCode#
uint16_t EmberAfClusterCommand::mfgCode
Definition at line
439
of file app/framework/include/af-types.h
seqNum#
uint8_t EmberAfClusterCommand::seqNum
Definition at line
440
of file app/framework/include/af-types.h
commandId#
uint8_t EmberAfClusterCommand::commandId
Definition at line
441
of file app/framework/include/af-types.h
payloadStartIndex#
uint8_t EmberAfClusterCommand::payloadStartIndex
Definition at line
442
of file app/framework/include/af-types.h
direction#
uint8_t EmberAfClusterCommand::direction
Definition at line
443
of file app/framework/include/af-types.h
interPanHeader#
EmberAfInterpanHeader* EmberAfClusterCommand::interPanHeader
Definition at line
444
of file app/framework/include/af-types.h
networkIndex#
uint8_t EmberAfClusterCommand::networkIndex
Definition at line
445
of file app/framework/include/af-types.h