Debug Print#

API and Callbacks for the Debug Print Component.

API#

sl_zigbee_debug_print_enable_group(uint32_t group_type, bool enable)
void
sli_zigbee_debug_print_buffer(uint32_t group_type, const uint8_t *buffer, uint16_t buffer_length, bool with_space, const char *format_string)

Enumerations#

enum
SL_ZIGBEE_DEBUG_PRINT_TYPE_STACK = 0x01
SL_ZIGBEE_DEBUG_PRINT_TYPE_CORE = 0x02
SL_ZIGBEE_DEBUG_PRINT_TYPE_APP = 0x04
SL_ZIGBEE_DEBUG_PRINT_TYPE_ZCL = 0x08
SL_ZIGBEE_DEBUG_PRINT_TYPE_LEGACY_AF_DEBUG = 0x10
}

API Documentation#

sl_zigbee_debug_print_enable_group#

sl_status_t sl_zigbee_debug_print_enable_group (uint32_t group_type, bool enable)
Parameters
N/Agroup_type

Ver.: always

N/Aenable

value Ver.: always

Enable groups in debug prints.

Returns

  • sl_status_t status code


Definition at line 82 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sli_zigbee_debug_print_buffer#

void sli_zigbee_debug_print_buffer (uint32_t group_type, const uint8_t * buffer, uint16_t buffer_length, bool with_space, const char * format_string)
Parameters
N/Agroup_type

Ver.: always

N/Abuffer

value Ver.: always

N/Abuffer_length
N/Awith_space
N/Aformat_string

Enable groups in debug prints.

Returns

  • sl_status_t status code


Definition at line 84 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

Enumeration Documentation#

sl_zigbee_debug_print_type#

sl_zigbee_debug_print_type
Enumerator
SL_ZIGBEE_DEBUG_PRINT_TYPE_STACK
SL_ZIGBEE_DEBUG_PRINT_TYPE_CORE
SL_ZIGBEE_DEBUG_PRINT_TYPE_APP
SL_ZIGBEE_DEBUG_PRINT_TYPE_ZCL
SL_ZIGBEE_DEBUG_PRINT_TYPE_LEGACY_AF_DEBUG

Definition at line 62 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

Macro Definition Documentation#

local_printf#

#define local_printf
Value:
printf

Definition at line 55 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

local_vprintf#

#define local_vprintf
Value:
vprintf

Definition at line 56 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_stack_debug_print#

#define sl_zigbee_stack_debug_print

Definition at line 98 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_stack_debug_println#

#define sl_zigbee_stack_debug_println

Definition at line 99 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_stack_debug_print_buffer#

#define sl_zigbee_stack_debug_print_buffer

Definition at line 100 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_stack_debug_print_string#

#define sl_zigbee_stack_debug_print_string

Definition at line 101 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_stack_debug_print_long_string#

#define sl_zigbee_stack_debug_print_long_string

Definition at line 102 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_core_debug_print#

#define sl_zigbee_core_debug_print

Definition at line 112 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_core_debug_println#

#define sl_zigbee_core_debug_println

Definition at line 113 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_core_debug_print_buffer#

#define sl_zigbee_core_debug_print_buffer

Definition at line 114 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_core_debug_print_string#

#define sl_zigbee_core_debug_print_string

Definition at line 115 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_core_debug_print_long_string#

#define sl_zigbee_core_debug_print_long_string

Definition at line 116 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_app_debug_print#

#define sl_zigbee_app_debug_print

Definition at line 126 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_app_debug_println#

#define sl_zigbee_app_debug_println

Definition at line 127 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_app_debug_print_buffer#

#define sl_zigbee_app_debug_print_buffer

Definition at line 128 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_app_debug_print_string#

#define sl_zigbee_app_debug_print_string

Definition at line 129 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_app_debug_print_long_string#

#define sl_zigbee_app_debug_print_long_string

Definition at line 130 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_zcl_debug_print#

#define sl_zigbee_zcl_debug_print

Definition at line 140 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_zcl_debug_println#

#define sl_zigbee_zcl_debug_println

Definition at line 141 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_zcl_debug_print_buffer#

#define sl_zigbee_zcl_debug_print_buffer

Definition at line 142 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_zcl_debug_print_string#

#define sl_zigbee_zcl_debug_print_string

Definition at line 143 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_zcl_debug_print_long_string#

#define sl_zigbee_zcl_debug_print_long_string

Definition at line 144 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_legacy_af_debug_print#

#define sl_zigbee_legacy_af_debug_print

Definition at line 154 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_legacy_af_debug_println#

#define sl_zigbee_legacy_af_debug_println

Definition at line 155 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_legacy_af_debug_print_buffer#

#define sl_zigbee_legacy_af_debug_print_buffer

Definition at line 156 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_legacy_af_debug_print_string#

#define sl_zigbee_legacy_af_debug_print_string

Definition at line 157 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h

sl_zigbee_legacy_af_debug_print_long_string#

#define sl_zigbee_legacy_af_debug_print_long_string

Definition at line 158 of file app/framework/plugin/debug-print/sl_zigbee_debug_print.h