This is a unique identifier for referencing Zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.
Public Attribute Documentation#
manufacturerId#
uint16_t EmberAfOtaImageId::manufacturerId
Definition at line
1212
of file app/framework/include/af-types.h
imageTypeId#
uint16_t EmberAfOtaImageId::imageTypeId
Definition at line
1213
of file app/framework/include/af-types.h
firmwareVersion#
uint32_t EmberAfOtaImageId::firmwareVersion
Definition at line
1214
of file app/framework/include/af-types.h
deviceSpecificFileEui64#
uint8_t EmberAfOtaImageId::deviceSpecificFileEui64[EUI64_SIZE]
This is only used for device-specific files. It will be set to all zeroes when the image does not have an upgrade destination field in it. Little endian format.
Definition at line
1222
of file app/framework/include/af-types.h