Public Attributes#

uint32_t
uint16_t

Public Attribute Documentation#

bitmask#

uint32_t EmberTokTypeStackZllData::bitmask

Definition at line 272 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

freeNodeIdMin#

uint16_t EmberTokTypeStackZllData::freeNodeIdMin

Definition at line 273 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

freeNodeIdMax#

uint16_t EmberTokTypeStackZllData::freeNodeIdMax

Definition at line 274 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

myGroupIdMin#

uint16_t EmberTokTypeStackZllData::myGroupIdMin

Definition at line 275 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

freeGroupIdMin#

uint16_t EmberTokTypeStackZllData::freeGroupIdMin

Definition at line 276 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

freeGroupIdMax#

uint16_t EmberTokTypeStackZllData::freeGroupIdMax

Definition at line 277 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h

rssiCorrection#

uint8_t EmberTokTypeStackZllData::rssiCorrection

Definition at line 278 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/zll-types.h