Public Attributes#

uint16_t
uint16_t
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@11
struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@12
union EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10

Public Attribute Documentation#

totalLengthOfAddInfoBlock#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::totalLengthOfAddInfoBlock

Definition at line 518 of file stack/include/gp-types.h

optionSelector#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::optionSelector

Definition at line 519 of file stack/include/gp-types.h

reportIdentifier#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::reportIdentifier

Definition at line 522 of file stack/include/gp-types.h

attrOffsetWithinReport#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attrOffsetWithinReport

Definition at line 523 of file stack/include/gp-types.h

clusterID#

uint16_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::clusterID

Definition at line 524 of file stack/include/gp-types.h

attributeID#

uint16_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attributeID

Definition at line 525 of file stack/include/gp-types.h

attributeDataType#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attributeDataType

Definition at line 526 of file stack/include/gp-types.h

attributeOptions#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::attributeOptions

Definition at line 527 of file stack/include/gp-types.h

manufacturerID#

uint16_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::manufacturerID

Definition at line 528 of file stack/include/gp-types.h

compactAttr#

struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@11 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::compactAttr

Definition at line 529 of file stack/include/gp-types.h

contactStatus#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::contactStatus

Definition at line 533 of file stack/include/gp-types.h

contactBitmask#

uint8_t EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::contactBitmask

Definition at line 535 of file stack/include/gp-types.h

genericSwitch#

struct EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10::@12 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::genericSwitch

Definition at line 536 of file stack/include/gp-types.h

optionData#

union EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::@10 EmberGpTranslationTableAdditionalInfoBlockOptionRecordField::optionData

Definition at line 537 of file stack/include/gp-types.h