This data structure contains the transient key data that is used during Zigbee 3.0 joining.
Public Attributes#
union EmberTransientKeyData::@2
Public Attribute Documentation#
eui64#
EmberEUI64 EmberTransientKeyData::eui64
incomingFrameCounter#
uint32_t EmberTransientKeyData::incomingFrameCounter
bitmask#
EmberKeyStructBitmask EmberTransientKeyData::bitmask
remainingTimeSeconds#
uint16_t EmberTransientKeyData::remainingTimeSeconds
networkIndex#
uint8_t EmberTransientKeyData::networkIndex
keyData#
EmberKeyData EmberTransientKeyData::keyData
psa_id#
uint32_t EmberTransientKeyData::psa_id
union EmberTransientKeyData::@2 EmberTransientKeyData::@3