This data structure contains the transient key data that is used during Zigbee 3.0 joining.

Public Attributes#

EmberEUI64
uint32_t
union EmberTransientKeyData::@2

Public Attribute Documentation#

eui64#

EmberEUI64 EmberTransientKeyData::eui64

Definition at line 2204 of file stack/include/ember-types.h

incomingFrameCounter#

uint32_t EmberTransientKeyData::incomingFrameCounter

Definition at line 2205 of file stack/include/ember-types.h

bitmask#

EmberKeyStructBitmask EmberTransientKeyData::bitmask

Definition at line 2206 of file stack/include/ember-types.h

remainingTimeSeconds#

uint16_t EmberTransientKeyData::remainingTimeSeconds

Definition at line 2207 of file stack/include/ember-types.h

networkIndex#

uint8_t EmberTransientKeyData::networkIndex

Definition at line 2208 of file stack/include/ember-types.h

keyData#

EmberKeyData EmberTransientKeyData::keyData

Definition at line 2210 of file stack/include/ember-types.h

psa_id#

uint32_t EmberTransientKeyData::psa_id

Definition at line 2211 of file stack/include/ember-types.h

@3#

union EmberTransientKeyData::@2 EmberTransientKeyData::@3

Definition at line 2212 of file stack/include/ember-types.h