Defines an entry in the binding table.
A binding entry specifies a local endpoint, a remote endpoint, a cluster ID and either the destination EUI64 (for unicast bindings) or the 64-bit group address (for multicast bindings).
Public Attribute Documentation#
type#
EmberBindingType EmberBindingTableEntry::type
The type of binding.
1322
of file stack/include/ember-types.h
local#
uint8_t EmberBindingTableEntry::local
The endpoint on the local node.
1324
of file stack/include/ember-types.h
clusterId#
uint16_t EmberBindingTableEntry::clusterId
A cluster ID that matches one from the local endpoint's simple descriptor. This cluster ID is set by the provisioning application to indicate which part an endpoint's functionality is bound to this particular remote node and is used to distinguish between unicast and multicast bindings. Note that a binding can be used to to send messages with any cluster ID, not just that listed in the binding.
1332
of file stack/include/ember-types.h
remote#
uint8_t EmberBindingTableEntry::remote
The endpoint on the remote node (specified by identifier
).
1334
of file stack/include/ember-types.h
identifier#
EmberEUI64 EmberBindingTableEntry::identifier
A 64-bit identifier. This is either:
The destination EUI64, for unicasts.
A 16-bit multicast group address, for multicasts.
1339
of file stack/include/ember-types.h
networkIndex#
uint8_t EmberBindingTableEntry::networkIndex
The index of the network the binding belongs to.
1341
of file stack/include/ember-types.h