Public Attribute Documentation#

deviceId#

uint8_t EmberGpApplicationInfo::deviceId

Definition at line 448 of file stack/include/gp-types.h

applInfoBitmap#

uint8_t EmberGpApplicationInfo::applInfoBitmap

Definition at line 449 of file stack/include/gp-types.h

manufacturerId#

uint16_t EmberGpApplicationInfo::manufacturerId

Definition at line 450 of file stack/include/gp-types.h

modelId#

uint16_t EmberGpApplicationInfo::modelId

Definition at line 451 of file stack/include/gp-types.h

numberOfGpdCommands#

uint8_t EmberGpApplicationInfo::numberOfGpdCommands

Definition at line 452 of file stack/include/gp-types.h

gpdCommands#

uint8_t EmberGpApplicationInfo::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]

Definition at line 453 of file stack/include/gp-types.h

numberOfPairedEndpoints#

uint8_t EmberGpApplicationInfo::numberOfPairedEndpoints

Definition at line 454 of file stack/include/gp-types.h

pairedEndpoints#

uint8_t EmberGpApplicationInfo::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]

Definition at line 455 of file stack/include/gp-types.h

numberOfGpdClientCluster#

uint8_t EmberGpApplicationInfo::numberOfGpdClientCluster

Definition at line 456 of file stack/include/gp-types.h

numberOfGpdServerCluster#

uint8_t EmberGpApplicationInfo::numberOfGpdServerCluster

Definition at line 457 of file stack/include/gp-types.h

serverClusters#

uint16_t EmberGpApplicationInfo::serverClusters[15]

Definition at line 458 of file stack/include/gp-types.h

clientClusters#

uint16_t EmberGpApplicationInfo::clientClusters[15]

Definition at line 459 of file stack/include/gp-types.h