Application information. During the commissioning of GPD that supports generic switch, multi sensor extension and compact report attribute the application information is exchanged as part of the GPD commissioning command 0xE0 and 0xE4. This structure holds the information for the commissioned GPD.

Public Attribute Documentation#

deviceId#

uint8_t EmberGpApplicationInfo::deviceId

Device ID of the GPD


Definition at line 495 of file stack/include/gp-types.h

applInfoBitmap#

uint8_t EmberGpApplicationInfo::applInfoBitmap

Application Information bitmap


Definition at line 497 of file stack/include/gp-types.h

manufacturerId#

uint16_t EmberGpApplicationInfo::manufacturerId

Manufacturer ID of the GPD


Definition at line 499 of file stack/include/gp-types.h

modelId#

uint16_t EmberGpApplicationInfo::modelId

Model ID of the GPD


Definition at line 501 of file stack/include/gp-types.h

numberOfGpdCommands#

uint8_t EmberGpApplicationInfo::numberOfGpdCommands

Number of GPD commands supported by the GPD


Definition at line 503 of file stack/include/gp-types.h

gpdCommands#

uint8_t EmberGpApplicationInfo::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]

Supported GPD Commands


Definition at line 505 of file stack/include/gp-types.h

numberOfPairedEndpoints#

uint8_t EmberGpApplicationInfo::numberOfPairedEndpoints

Number of paired endpoints for the GPD


Definition at line 507 of file stack/include/gp-types.h

pairedEndpoints#

uint8_t EmberGpApplicationInfo::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]

Paired endpoints


Definition at line 509 of file stack/include/gp-types.h

numberOfGpdClientCluster#

uint8_t EmberGpApplicationInfo::numberOfGpdClientCluster

Number of operational client clusters present on the GPD, maximum is 15.


Definition at line 511 of file stack/include/gp-types.h

numberOfGpdServerCluster#

uint8_t EmberGpApplicationInfo::numberOfGpdServerCluster

Number of operational server clusters present on the GPD, maximum is 15.


Definition at line 513 of file stack/include/gp-types.h

serverClusters#

uint16_t EmberGpApplicationInfo::serverClusters[15]

Operational server clusters present on the GPD


Definition at line 515 of file stack/include/gp-types.h

clientClusters#

uint16_t EmberGpApplicationInfo::clientClusters[15]

Operational client clusters present on the GPD


Definition at line 517 of file stack/include/gp-types.h