Zigbee Green Power types and defines. See greenpower for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_GP_TYPES_H
#define SILABS_GP_TYPES_H
// Mask used in the Gp Ep Incoming Message Handler to pass bidirectional information
// Incoming GPDF has rxAfterTx bit set
#define EMBER_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASK 0x01
// A tx queue is available at gp stub to hold an outgoing GPDF
#define EMBER_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASK 0x02
typedef uint32_t EmberGpSourceId;
typedef uint32_t EmberGpSecurityFrameCounter;
typedef uint32_t EmberGpMic;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberGpSecurityLevel
#else
typedef uint8_t EmberGpSecurityLevel;
enum
#endif
{
EMBER_GP_SECURITY_LEVEL_NONE = 0x00,
EMBER_GP_SECURITY_LEVEL_RESERVED = 0x01,
EMBER_GP_SECURITY_LEVEL_FC_MIC = 0x02,
EMBER_GP_SECURITY_LEVEL_FC_MIC_ENCRYPTED = 0x03,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberGpKeyType
#else
typedef uint8_t EmberGpKeyType;
enum
#endif
{
EMBER_GP_SECURITY_KEY_NONE = 0x00,
EMBER_GP_SECURITY_KEY_NWK = 0x01,
EMBER_GP_SECURITY_KEY_GPD_GROUP = 0x02,
EMBER_GP_SECURITY_KEY_NWK_DERIVED = 0x03,
EMBER_GP_SECURITY_KEY_GPD_OOB = 0x04,
EMBER_GP_SECURITY_KEY_GPD_DERIVED = 0x07,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberGpApplicationId
#else
typedef uint8_t EmberGpApplicationId;
enum
#endif
{
EMBER_GP_APPLICATION_SOURCE_ID = 0x00,
EMBER_GP_APPLICATION_IEEE_ADDRESS = 0x02,
};
#define EMBER_GP_APPLICATION_ID_MASK 0x03
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberGpProxyTableEntryStatus
#else
typedef uint8_t EmberGpProxyTableEntryStatus;
enum
#endif
{
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_ACTIVE = 0x01,
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_UNUSED = 0xFF,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberGpSinkTableEntryStatus
#else
typedef uint8_t EmberGpSinkTableEntryStatus;
enum
#endif
{
EMBER_GP_SINK_TABLE_ENTRY_STATUS_ACTIVE = 0x01,
EMBER_GP_SINK_TABLE_ENTRY_STATUS_UNUSED = 0xFF,
};
typedef struct {
union {
EmberEUI64 gpdIeeeAddress;
EmberGpSourceId sourceId;
} id;
EmberGpApplicationId applicationId;
uint8_t endpoint;
} EmberGpAddress;
typedef enum {
EMBER_GP_SINK_TYPE_FULL_UNICAST,
EMBER_GP_SINK_TYPE_D_GROUPCAST,
EMBER_GP_SINK_TYPE_GROUPCAST,
EMBER_GP_SINK_TYPE_LW_UNICAST,
EMBER_GP_SINK_TYPE_UNUSED = 0xFF
} EmberGpSinkType;
typedef struct {
EmberEUI64 sinkEUI;
EmberNodeId sinkNodeId;
} EmberGpSinkAddress;
typedef struct {
uint16_t groupID;
uint16_t alias;
} EmberGpSinkGroup;
typedef struct {
EmberGpSinkType type;
union {
EmberGpSinkAddress unicast;
EmberGpSinkGroup groupcast;
EmberGpSinkGroup groupList; // Entry for Sink Group List
} target;
} EmberGpSinkListEntry;
#define GP_SINK_LIST_ENTRIES 2
// The size of the SinkList entries in sink table in format of octet string that has a format of {<1 byte length>, <n bytes for sink groups>}
#define GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRING (1 + (GP_SINK_LIST_ENTRIES * (sizeof(EmberGpSinkGroup))))
typedef struct {
EmberGpProxyTableEntryStatus status;
uint32_t options;
EmberGpAddress gpd;
EmberNodeId assignedAlias;
uint8_t securityOptions;
EmberGpSecurityFrameCounter gpdSecurityFrameCounter;
EmberKeyData gpdKey;
EmberGpSinkListEntry sinkList[GP_SINK_LIST_ENTRIES];
uint8_t groupcastRadius;
uint8_t searchCounter;
} EmberGpProxyTableEntry;
typedef struct {
EmberGpSinkTableEntryStatus status;
uint16_t options;
EmberGpAddress gpd;
uint8_t deviceId;
EmberGpSinkListEntry sinkList[GP_SINK_LIST_ENTRIES];
EmberNodeId assignedAlias;
uint8_t groupcastRadius;
uint8_t securityOptions;
EmberGpSecurityFrameCounter gpdSecurityFrameCounter;
EmberKeyData gpdKey;
} EmberGpSinkTableEntry;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberCGpTxOption
#else
typedef uint8_t EmberCGpTxOption;
enum
#endif
{
EMBER_CGP_TX_OPTION_NONE = 0x00,
EMBER_CGP_TX_OPTION_USE_CSMA_CA = 0x01,
EMBER_CGP_TX_OPTION_USE_MAC_ACK = 0x02,
EMBER_CGP_TX_OPTION_RESERVED = 0xFC,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberCGpAddressMode
#else
typedef uint8_t EmberCGpAddressMode;
enum
#endif
{
EMBER_CGP_ADDRESS_MODE_NONE = 0x00,
EMBER_CGP_ADDRESS_MODE_RESERVED = 0x01,
EMBER_CGP_ADDRESS_MODE_SHORT = 0x02,
EMBER_CGP_ADDRESS_MODE_EXTENDED = 0x03,
};
typedef struct {
union {
EmberNodeId shortId;
EmberEUI64 extendedId;
} address;
EmberPanId panId;
EmberCGpAddressMode mode;
} EmberCGpAddress;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberDGpTxOption
#else
typedef uint8_t EmberDGpTxOption;
enum
#endif
{
EMBER_DGP_TX_OPTION_NONE = 0x00,
EMBER_DGP_TX_OPTION_USE_GP_TX_QUEUE = 0x01,
EMBER_DGP_TX_OPTION_USE_CSMA_CA = 0x02,
EMBER_DGP_TX_OPTION_USE_MAC_ACK = 0x04,
EMBER_DGP_TX_OPTION_FRAME_TYPE_DATA = 0x00,
EMBER_DGP_TX_OPTION_FRAME_TYPE_MAINTENANCE = 0x08,
EMBER_DGP_TX_OPTION_RESERVED = 0xE0,
};
typedef struct {
uint8_t foo;
} EmberGpProxyClusterAttributes;
typedef struct {
bool inUse;
bool useCca;
EmberGpAddress addr;
uint8_t gpdCommandId;
EmberMessageBuffer asdu;
uint8_t gpepHandle;
uint16_t queueEntryLifetimeMs;
} EmberGpTxQueueEntry;
#define GP_PARAMS \
EmberStatus status, \
uint8_t gpdLink, \
uint8_t sequenceNumber, \
EmberGpAddress * addr, \
EmberGpSecurityLevel gpdfSecurityLevel, \
EmberGpKeyType gpdfSecurityKeyType, \
bool autoCommissioning, \
uint8_t bidirectionalInfo, \
uint32_t gpdSecurityFrameCounter, \
uint8_t gpdCommandId, \
uint32_t mic, \
uint8_t proxyTableIndex, \
uint8_t gpdCommandPayloadLength, \
uint8_t * gpdCommandPayload
#define GP_ARGS \
status, \
gpdLink, \
sequenceNumber, \
addr, \
gpdfSecurityLevel, \
gpdfSecurityKeyType, \
autoCommissioning, \
bidirectionalInfo, \
gpdSecurityFrameCounter, \
gpdCommandId, \
mic, \
proxyTableIndex, \
gpdCommandPayloadLength, \
gpdCommandPayload
#define GP_UNUSED_ARGS \
(void)status; \
(void)gpdLink; \
(void)sequenceNumber; \
(void)addr; \
(void)gpdfSecurityLevel; \
(void)gpdfSecurityKeyType; \
(void)autoCommissioning; \
(void)rxAfterTx; \
(void)gpdSecurityFrameCounter; \
(void)gpdCommandId; \
(void)mic; \
(void)proxyTableIndex; \
(void)gpdCommandPayloadLength; \
(void)gpdCommandPayload;
#define GP_PROXY_TABLE_OPTIONS_IN_RANGE (BIT(10))
//3 consumed by device id, options, and app info byte
#define GP_COMMISSIONING_MAX_BYTES (55 - 3)
typedef struct {
uint8_t deviceId;
uint8_t applInfoBitmap;
uint16_t manufacturerId;
uint16_t modelId;
uint8_t numberOfGpdCommands;
uint8_t gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1];
uint8_t numberOfPairedEndpoints;
uint8_t pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1];
uint8_t numberOfGpdClientCluster;
uint8_t numberOfGpdServerCluster;
uint16_t serverClusters[15];
uint16_t clientClusters[15];
} EmberGpApplicationInfo;
typedef struct {
uint16_t attributeID;
uint8_t attributeDataType;
uint8_t remainingAttributRecordLength; // on 4 bits
uint8_t reported;
uint8_t attrValuePresent;
uint8_t attrOffsetWithinReport;
// TODO change "attrValue" from u32 to a pointer, as the data could be up to a string
// the field "attributeDataType" tell with format it is, among more than 55 possibilities)
// so a add a private field which just tell the length of attrValue to easier
// process it
uint32_t attrValue;
uint8_t attrValueSize;
} EmberGpAttributeRecord;
typedef struct {
// Note: it is "N-1", if there is 2 attr record then nbAttrRecord=1 and not 2 !
uint8_t nbAttrRecord;
uint8_t clientServer;
uint8_t ManIdPresent;
uint8_t datapointOptions;
uint16_t clusterID;
uint16_t manufacturerID;
EmberGpAttributeRecord attrRecord;
} EmberGpDataPointDescriptor;
typedef struct {
uint8_t repId;
uint8_t reportOptions;
uint16_t timeoutPeriod;
uint8_t totalLength;
EmberGpDataPointDescriptor dataPoint;
} EmberGpReportDescriptor;
typedef struct {
uint8_t switchInfoLength;
uint8_t nbOfContacts;
uint8_t switchType;
uint8_t currentContact;
uint8_t savedContact;
}EmberGpSwitchInformation;
#define TT_NB_MAX_OPTION_RECORD (8)
typedef struct {
uint8_t currentStatus;
uint8_t contactBitmask;
} EmberGpGenericSwitchData;
typedef struct {
uint8_t totalLengthOfAddInfoBlock;
uint8_t optionSelector;
union {
struct {
uint8_t reportIdentifier;
uint8_t attrOffsetWithinReport;
uint16_t clusterID;
uint16_t attributeID;
uint8_t attributeDataType;
uint8_t attributeOptions; //clientServer bit0 manufacturerIdPresent bit1
uint16_t manufacturerID;
} compactAttr;
struct {
uint8_t contactStatus;
uint8_t contactBitmask;
} genericSwitch;
} optionData;//EmberGpTranslationTableAdditionalInfoBlockOptionRecordOptionDataField;
} EmberGpTranslationTableAdditionalInfoBlockOptionRecordField;
#define GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIG 0x00000000
#define GP_GPD_SRC_ID_WILDCARD 0xFFFFFFFF
// GPD SrcID reserved values
#define GP_GPD_SRC_ID_RESERVED_0 0x00000000
#define GP_GPD_SRC_ID_RESERVED_FFFFFF9 0xFFFFFFF9
#define GP_GPD_SRC_ID_RESERVED_FFFFFFA 0xFFFFFFFA
#define GP_GPD_SRC_ID_RESERVED_FFFFFFB 0xFFFFFFFB
#define GP_GPD_SRC_ID_RESERVED_FFFFFFC 0xFFFFFFFC
#define GP_GPD_SRC_ID_RESERVED_FFFFFFD 0xFFFFFFFD
#define GP_GPD_SRC_ID_RESERVED_FFFFFFE 0xFFFFFFFE
#define GP_DERIVED_GROUP_ALIAS_NOT_USED 0xffff
#define GP_DMIN_B 32
#define GP_DMIN_U 5
#define GP_DMAX 100
// -----------------------------------------------------------------------------
// API
EmberStatus emberDGpSend(bool action,
bool useCca,
EmberGpAddress *addr,
uint8_t gpdCommandId,
uint8_t gpdAsduLength,
uint8_t const *gpdAsdu,
uint8_t gpepHandle,
uint16_t gpTxQueueEntryLifetimeMs);
// Tx Queue APIs
MessageBufferQueue * emberGpGetTxQueueHead(void);
void emberGpSetMaxTxQueueEntry(uint16_t maxEntries);
uint16_t emberGetGpMaxTxQListCount(void);
uint16_t emberGetGpTxQListCount(void);
EmberMessageBuffer emberGpGetTxQueueEntryFromQueue(EmberGpTxQueueEntry *txQueue,
uint8_t *data,
uint16_t *dataLength,
uint16_t allocatedDataLength);
EmberMessageBuffer emberGpAddGpTxQueueEntryWithPayload(EmberGpTxQueueEntry *txQueue,
uint8_t *data,
uint16_t dataLength);
bool emberGpRemoveFromTxQueue(EmberGpTxQueueEntry *txQueue);
void emberGpClearTxQueue(void);
#endif // SILABS_GP_TYPES_H
// end of name API
Modules#
EmberGpTranslationTableAdditionalInfoBlockOptionRecordField
GP Types#
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of maximum option record entries in translation table.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Number of GP sink list entries. Minimum is 2 sink list entries.
Green Power Security Level.
Green Power Security Security Key Type.
Green Power Application Id.
GP proxy table entry status.
GP sink table entry status.
GP Sink Type.
CGp Transmit options.
Addressing modes for CGp messages.
Transmit options for DGp messages.
API#
DGp Send.
Gets tx queue head.
Sets maximum limit for number of entries in the tx queue.
Gets the limit set for maximum number of entries in the tx queue.
Gets the number of entries in the tx queue.
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns EMBER_NULL_MESSAGE_BUFFER if not found.
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
Remove an entry from Tx Queue This function searches and removes the entry provided.
Purges Tx Queue This function purges the tx queue.
Macros#
GP Types Documentation#
EMBER_GP_APPLICATION_ID_MASK#
#define EMBER_GP_APPLICATION_ID_MASKValue:
0x03
Number of GP sink list entries. Minimum is 2 sink list entries.
105
of file stack/include/gp-types.h
GP_SINK_LIST_ENTRIES#
#define GP_SINK_LIST_ENTRIESValue:
2
Number of GP sink list entries. Minimum is 2 sink list entries.
225
of file stack/include/gp-types.h
GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRING#
#define GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRINGValue:
(1 + (GP_SINK_LIST_ENTRIES * (sizeof(EmberGpSinkGroup))))
Number of GP sink list entries. Minimum is 2 sink list entries.
228
of file stack/include/gp-types.h
GP_PARAMS#
#define GP_PARAMSValue:
Number of GP sink list entries. Minimum is 2 sink list entries.
434
of file stack/include/gp-types.h
GP_ARGS#
#define GP_ARGSValue:
Number of GP sink list entries. Minimum is 2 sink list entries.
450
of file stack/include/gp-types.h
GP_UNUSED_ARGS#
#define GP_UNUSED_ARGSValue:
Number of GP sink list entries. Minimum is 2 sink list entries.
466
of file stack/include/gp-types.h
GP_PROXY_TABLE_OPTIONS_IN_RANGE#
#define GP_PROXY_TABLE_OPTIONS_IN_RANGEValue:
(BIT(10))
Number of GP sink list entries. Minimum is 2 sink list entries.
482
of file stack/include/gp-types.h
GP_COMMISSIONING_MAX_BYTES#
#define GP_COMMISSIONING_MAX_BYTESValue:
(55 - 3)
Number of GP sink list entries. Minimum is 2 sink list entries.
485
of file stack/include/gp-types.h
TT_NB_MAX_OPTION_RECORD#
#define TT_NB_MAX_OPTION_RECORDValue:
(8)
Number of maximum option record entries in translation table.
610
of file stack/include/gp-types.h
GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIG#
#define GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIGValue:
0x00000000
Number of GP sink list entries. Minimum is 2 sink list entries.
659
of file stack/include/gp-types.h
GP_GPD_SRC_ID_WILDCARD#
#define GP_GPD_SRC_ID_WILDCARDValue:
0xFFFFFFFF
Number of GP sink list entries. Minimum is 2 sink list entries.
660
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_0#
#define GP_GPD_SRC_ID_RESERVED_0Value:
0x00000000
Number of GP sink list entries. Minimum is 2 sink list entries.
663
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFF9#
#define GP_GPD_SRC_ID_RESERVED_FFFFFF9Value:
0xFFFFFFF9
Number of GP sink list entries. Minimum is 2 sink list entries.
664
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFA#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFAValue:
0xFFFFFFFA
Number of GP sink list entries. Minimum is 2 sink list entries.
665
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFB#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFBValue:
0xFFFFFFFB
Number of GP sink list entries. Minimum is 2 sink list entries.
666
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFC#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFCValue:
0xFFFFFFFC
Number of GP sink list entries. Minimum is 2 sink list entries.
667
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFD#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFDValue:
0xFFFFFFFD
Number of GP sink list entries. Minimum is 2 sink list entries.
668
of file stack/include/gp-types.h
GP_GPD_SRC_ID_RESERVED_FFFFFFE#
#define GP_GPD_SRC_ID_RESERVED_FFFFFFEValue:
0xFFFFFFFE
Number of GP sink list entries. Minimum is 2 sink list entries.
669
of file stack/include/gp-types.h
GP_DERIVED_GROUP_ALIAS_NOT_USED#
#define GP_DERIVED_GROUP_ALIAS_NOT_USEDValue:
0xffff
Number of GP sink list entries. Minimum is 2 sink list entries.
671
of file stack/include/gp-types.h
GP_DMIN_B#
#define GP_DMIN_BValue:
32
Number of GP sink list entries. Minimum is 2 sink list entries.
673
of file stack/include/gp-types.h
GP_DMIN_U#
#define GP_DMIN_UValue:
5
Number of GP sink list entries. Minimum is 2 sink list entries.
674
of file stack/include/gp-types.h
GP_DMAX#
#define GP_DMAXValue:
100
Number of GP sink list entries. Minimum is 2 sink list entries.
675
of file stack/include/gp-types.h
EmberGpSecurityLevel#
EmberGpSecurityLevel
Green Power Security Level.
Enumerator | |
---|---|
EMBER_GP_SECURITY_LEVEL_NONE | No Security |
EMBER_GP_SECURITY_LEVEL_RESERVED | Reserved |
EMBER_GP_SECURITY_LEVEL_FC_MIC | 4 Byte Frame Counter and 4 Byte MIC |
EMBER_GP_SECURITY_LEVEL_FC_MIC_ENCRYPTED | 4 Byte Frame Counter and 4 Byte MIC with encryption |
51
of file stack/include/gp-types.h
EmberGpKeyType#
EmberGpKeyType
Green Power Security Security Key Type.
Enumerator | |
---|---|
EMBER_GP_SECURITY_KEY_NONE | No Key |
EMBER_GP_SECURITY_KEY_NWK | GP Security Key Type is Zigbee Network Key |
EMBER_GP_SECURITY_KEY_GPD_GROUP | GP Security Key Type is Group Key |
EMBER_GP_SECURITY_KEY_NWK_DERIVED | GP Security Key Type is Derived Network Key |
EMBER_GP_SECURITY_KEY_GPD_OOB | GP Security Key Type is Out Of Box Key |
EMBER_GP_SECURITY_KEY_GPD_DERIVED | GP Security Key Type is GPD Derived Key |
70
of file stack/include/gp-types.h
EmberGpApplicationId#
EmberGpApplicationId
Green Power Application Id.
Enumerator | |
---|---|
EMBER_GP_APPLICATION_SOURCE_ID | Source identifier. |
EMBER_GP_APPLICATION_IEEE_ADDRESS | IEEE address. |
93
of file stack/include/gp-types.h
EmberGpProxyTableEntryStatus#
EmberGpProxyTableEntryStatus
GP proxy table entry status.
Enumerator | |
---|---|
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_ACTIVE | The GP table entry is in use for a Proxy Table Entry. |
EMBER_GP_PROXY_TABLE_ENTRY_STATUS_UNUSED | The proxy table entry is not in use. |
110
of file stack/include/gp-types.h
EmberGpSinkTableEntryStatus#
EmberGpSinkTableEntryStatus
GP sink table entry status.
Enumerator | |
---|---|
EMBER_GP_SINK_TABLE_ENTRY_STATUS_ACTIVE | The GP table entry is in use for a Sink Table Entry. |
EMBER_GP_SINK_TABLE_ENTRY_STATUS_UNUSED | The proxy table entry is not in use. |
130
of file stack/include/gp-types.h
EmberGpSinkType#
EmberGpSinkType
GP Sink Type.
Enumerator | |
---|---|
EMBER_GP_SINK_TYPE_FULL_UNICAST | Sink Type is Full Unicast |
EMBER_GP_SINK_TYPE_D_GROUPCAST | Sink Type is Derived groupcast, the group ID is derived from the GpdId during commissioning. The sink is added to the APS group with that groupId. |
EMBER_GP_SINK_TYPE_GROUPCAST | Sink type EMBER_GP_SINK_TYPE_GROUPCAST, the groupId can be obtained from the APS group table or from the sink table. |
EMBER_GP_SINK_TYPE_LW_UNICAST | Sink Type is Light Weight Unicast. |
EMBER_GP_SINK_TYPE_UNUSED | Unused sink type |
171
of file stack/include/gp-types.h
EmberCGpTxOption#
EmberCGpTxOption
CGp Transmit options.
Enumerator | |
---|---|
EMBER_CGP_TX_OPTION_NONE | No options. |
EMBER_CGP_TX_OPTION_USE_CSMA_CA | Use CSMA/CA. |
EMBER_CGP_TX_OPTION_USE_MAC_ACK | Use MAC ACK. |
EMBER_CGP_TX_OPTION_RESERVED | Reserved. |
326
of file stack/include/gp-types.h
EmberCGpAddressMode#
EmberCGpAddressMode
Addressing modes for CGp messages.
Enumerator | |
---|---|
EMBER_CGP_ADDRESS_MODE_NONE | No address (PAN identifier and address omitted). |
EMBER_CGP_ADDRESS_MODE_RESERVED | Reserved. |
EMBER_CGP_ADDRESS_MODE_SHORT | 16-bit short address. |
EMBER_CGP_ADDRESS_MODE_EXTENDED | 64-bit extended address. |
346
of file stack/include/gp-types.h
EmberDGpTxOption#
EmberDGpTxOption
Transmit options for DGp messages.
Enumerator | |
---|---|
EMBER_DGP_TX_OPTION_NONE | No options. |
EMBER_DGP_TX_OPTION_USE_GP_TX_QUEUE | Use gpTxQueue. |
EMBER_DGP_TX_OPTION_USE_CSMA_CA | Use CSMA/CA. |
EMBER_DGP_TX_OPTION_USE_MAC_ACK | Use MAC ACK. |
EMBER_DGP_TX_OPTION_FRAME_TYPE_DATA | Data frame. |
EMBER_DGP_TX_OPTION_FRAME_TYPE_MAINTENANCE | Maintenance frame. |
EMBER_DGP_TX_OPTION_RESERVED | Reserved. |
388
of file stack/include/gp-types.h
EmberGpSourceId#
typedef uint32_t EmberGpSourceId
32-bit GPD source identifier
41
of file stack/include/gp-types.h
EmberGpSecurityFrameCounter#
typedef uint32_t EmberGpSecurityFrameCounter
32-bit security frame counter
43
of file stack/include/gp-types.h
EmberGpMic#
typedef uint32_t EmberGpMic
32-bit MIC code
45
of file stack/include/gp-types.h
API Documentation#
emberDGpSend#
EmberStatus emberDGpSend (bool action, bool useCca, EmberGpAddress * addr, uint8_t gpdCommandId, uint8_t gpdAsduLength, uint8_t const * gpdAsdu, uint8_t gpepHandle, uint16_t gpTxQueueEntryLifetimeMs)
DGp Send.
N/A | action | Action to add (true) or remove (false) |
N/A | useCca | Use CCA for GPDF transmission. |
N/A | addr | The gpd address EmberGpAddress. |
N/A | gpdCommandId | GPD Command ID |
N/A | gpdAsduLength | ASDU Length. |
N/A | gpdAsdu | The ASDU buffer that holds the outgoing GPDF as payload. |
N/A | gpepHandle | Handle for the asdu. |
N/A | gpTxQueueEntryLifetimeMs | Life time in milliseconds in Tx queue after which it gets cleared. |
This API adds or removes an outgoing GPDF (passed as ASDU) in the GP stub layer. As part of Gp Response command processing by green power client cluster, this API submits a outgoing a channel configuration or a commissioning reply GPDF. Similarly, it is called with appropriate action to clear the Tx queue upon channel request timeout.
Returns
An EmberStatus as status.
704
of file stack/include/gp-types.h
emberGpGetTxQueueHead#
MessageBufferQueue * emberGpGetTxQueueHead (void )
Gets tx queue head.
N/A |
This function gets the head pointer of the tx queue. Note : since it returns a pointer to memory the head, it 'll not be useful on host.
Returns
pointer to head of tx queue MessageBufferQueue
722
of file stack/include/gp-types.h
emberGpSetMaxTxQueueEntry#
void emberGpSetMaxTxQueueEntry (uint16_t maxEntries)
Sets maximum limit for number of entries in the tx queue.
N/A | maxEntries |
This function sets the maximum number of entries the tx queue is supposed to grow.
728
of file stack/include/gp-types.h
emberGetGpMaxTxQListCount#
uint16_t emberGetGpMaxTxQListCount (void )
Gets the limit set for maximum number of entries in the tx queue.
N/A |
This function gets the limit set for the maximum number of entries the tx queue is supposed to hold.
Returns
limit to the maximum number of entries.
736
of file stack/include/gp-types.h
emberGetGpTxQListCount#
uint16_t emberGetGpTxQListCount (void )
Gets the number of entries in the tx queue.
N/A |
This function gets the number of entries present in tx queue.
Returns
number of entries.
744
of file stack/include/gp-types.h
emberGpGetTxQueueEntryFromQueue#
EmberMessageBuffer emberGpGetTxQueueEntryFromQueue (EmberGpTxQueueEntry * txQueue, uint8_t * data, uint16_t * dataLength, uint16_t allocatedDataLength)
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns EMBER_NULL_MESSAGE_BUFFER if not found.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory to get a copy of the tx queue entry from the buffer queue. The caller populates the addr field of this parameter which is used as a search key. |
N/A | data | A pointer to an allocated memory to get a copy of the gpd command payload if an entry is found. This can be passed as NULL if payload is not required by caller. |
N/A | dataLength | A pointer to hold the length of the gpd command payload when an entry is found and the data collector is non-NULL. |
N/A | allocatedDataLength | Size in bytes for the allocated memory for the data collector. If this value is smaller compared to length of the data in the queue, no data gets copied out. |
Returns
Buffer EmberMessageBuffer that holds the entry if found, null message buffer if not found.
759
of file stack/include/gp-types.h
emberGpAddGpTxQueueEntryWithPayload#
EmberMessageBuffer emberGpAddGpTxQueueEntryWithPayload (EmberGpTxQueueEntry * txQueue, uint8_t * data, uint16_t dataLength)
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory holding the entry with all the members of the structure assigned as needed. |
N/A | data | A pointer holding the data payload. Can be supplied as NULL if there is no data payload. |
N/A | dataLength | Length of the data. |
Returns
Buffer EmberMessageBuffer that holds the entry upon success else null message buffer.
772
of file stack/include/gp-types.h
emberGpRemoveFromTxQueue#
bool emberGpRemoveFromTxQueue (EmberGpTxQueueEntry * txQueue)
Remove an entry from Tx Queue This function searches and removes the entry provided.
N/A | txQueue | EmberGpTxQueueEntry A pointer to an allocated memory holding the entry with gpd addr field assigned, which is used as for searching the tx queue. NOTE : Use of wildcard gpd addr (AppId = 0,SrcId = 0xFFFFFFFF) , removes all the entries of the tx queue. |
Returns
True upon success else false.
782
of file stack/include/gp-types.h
emberGpClearTxQueue#
void emberGpClearTxQueue (void )
Purges Tx Queue This function purges the tx queue.
N/A |
788
of file stack/include/gp-types.h
Macro Definition Documentation#
EMBER_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASK#
#define EMBER_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASKValue:
0x01
33
of file stack/include/gp-types.h
EMBER_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASK#
#define EMBER_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASKValue:
0x02
35
of file stack/include/gp-types.h