The internal representation of a sink table entry.
Public Attribute Documentation#
status#
EmberGpSinkTableEntryStatus EmberGpSinkTableEntry::status
Internal status. Defines if the entry is unused or used as a sink table entry
Definition at line
402
of file stack/include/gp-types.h
options#
uint16_t EmberGpSinkTableEntry::options
The tunneling options (this contains both options and extendedOptions from the spec)
Definition at line
406
of file stack/include/gp-types.h
gpd#
EmberGpAddress EmberGpSinkTableEntry::gpd
The addressing info of the GPD
Definition at line
410
of file stack/include/gp-types.h
deviceId#
uint8_t EmberGpSinkTableEntry::deviceId
The device ID for the GPD
Definition at line
414
of file stack/include/gp-types.h
sinkList#
EmberGpSinkListEntry EmberGpSinkTableEntry::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks; hardcoded to 2, which is the spec minimum
Definition at line
418
of file stack/include/gp-types.h
assignedAlias#
EmberNodeId EmberGpSinkTableEntry::assignedAlias
The assigned alias for the GPD
Definition at line
422
of file stack/include/gp-types.h
groupcastRadius#
uint8_t EmberGpSinkTableEntry::groupcastRadius
The groupcast radius
Definition at line
426
of file stack/include/gp-types.h
securityOptions#
uint8_t EmberGpSinkTableEntry::securityOptions
The security options field
Definition at line
430
of file stack/include/gp-types.h
gpdSecurityFrameCounter#
EmberGpSecurityFrameCounter EmberGpSinkTableEntry::gpdSecurityFrameCounter
The SFC of the GPD
Definition at line
434
of file stack/include/gp-types.h
gpdKey#
EmberKeyData EmberGpSinkTableEntry::gpdKey
The GPD key associated with this entry.
Definition at line
438
of file stack/include/gp-types.h