Holds network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit.
Public Attribute Documentation#
extendedPanId#
uint8_t EmberNetworkParameters::extendedPanId[EXTENDED_PAN_ID_SIZE]
The network's extended PAN identifier.
1266
of file stack/include/ember-types.h
panId#
uint16_t EmberNetworkParameters::panId
The network's PAN identifier.
1268
of file stack/include/ember-types.h
radioTxPower#
int8_t EmberNetworkParameters::radioTxPower
A power setting, in dBm.
1270
of file stack/include/ember-types.h
radioChannel#
uint8_t EmberNetworkParameters::radioChannel
A radio channel. Be sure to specify a channel supported by the radio.
1272
of file stack/include/ember-types.h
joinMethod#
EmberJoinMethod EmberNetworkParameters::joinMethod
Join method: The protocol messages used to establish an initial parent. It is ignored when forming a ZigBee network, or when querying the stack for its network parameters.
1277
of file stack/include/ember-types.h
nwkManagerId#
EmberNodeId EmberNetworkParameters::nwkManagerId
NWK Manager ID. The ID of the network manager in the current network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
1283
of file stack/include/ember-types.h
nwkUpdateId#
uint8_t EmberNetworkParameters::nwkUpdateId
An NWK Update ID. The value of the ZigBee nwkUpdateId known by the stack. It is used to determine the newest instance of the network after a PAN ID or channel change. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
1289
of file stack/include/ember-types.h
channels#
uint32_t EmberNetworkParameters::channels
The NWK channel mask. The list of preferred channels that the NWK manager has told this device to use when searching for the network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
1295
of file stack/include/ember-types.h