Information about the ZLL network and specific device that responded to a ZLL scan request.

Public Attribute Documentation#

zigbeeNetwork#

EmberZigbeeNetwork EmberZllNetwork::zigbeeNetwork

Definition at line 135 of file stack/include/zll-types.h

securityAlgorithm#

EmberZllSecurityAlgorithmData EmberZllNetwork::securityAlgorithm

Definition at line 136 of file stack/include/zll-types.h

eui64#

EmberEUI64 EmberZllNetwork::eui64

Definition at line 137 of file stack/include/zll-types.h

nodeId#

EmberNodeId EmberZllNetwork::nodeId

Definition at line 138 of file stack/include/zll-types.h

state#

EmberZllState EmberZllNetwork::state

Definition at line 139 of file stack/include/zll-types.h

nodeType#

EmberNodeType EmberZllNetwork::nodeType

Definition at line 140 of file stack/include/zll-types.h

numberSubDevices#

uint8_t EmberZllNetwork::numberSubDevices

Definition at line 141 of file stack/include/zll-types.h

totalGroupIdentifiers#

uint8_t EmberZllNetwork::totalGroupIdentifiers

Definition at line 142 of file stack/include/zll-types.h

rssiCorrection#

uint8_t EmberZllNetwork::rssiCorrection

Definition at line 143 of file stack/include/zll-types.h