Definitions for stack tokens. See Stack Tokens for documentation.

The file token-stack.h should not be included directly. It is accessed by the other token files.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#include "stack/include/sl_zigbee_types.h"

  #ifndef DEFINEADDRESSES
  #define TOKEN_NEXT_ADDRESS(region, address)
  #endif

// The basic TOKEN_DEF macro should not be used directly since the simplified
//  definitions are safer to use. For completeness of information, the basic
//  macro has the following format:
//
//  TOKEN_DEF(name,creator,iscnt,isidx,type,arraysize,...)
//  name - The root name used for the token
//  creator - a code used to uniquely identify the token
//  iscnt - a bool flag that is set to identify a counter token
//  isidx - a bool flag that is set to identify an indexed token
//  type - the basic type or typdef of the token
//  arraysize - the number of elements making up an indexed token
//  ... - initializers used when reseting the tokens to default values
//
//
// The following convenience macros are used to simplify the definition
//  process for commonly specified parameters to the basic TOKEN_DEF macro.
//  DEFINE_BASIC_TOKEN(name, type, ...)
//  DEFINE_INDEXED_TOKEN(name, type, arraysize, ...)
//  DEFINE_COUNTER_TOKEN(name, type, ...)
//  DEFINE_FIXED_BASIC_TOKEN(name, type, address, ...)
//  DEFINE_FIXED_INDEXED_TOKEN(name, type, arraysize, address, ...)
//  DEFINE_FIXED_COUNTER_TOKEN(name, type, address, ...)
//  DEFINE_MFG_TOKEN(name, type, address, ...)
//

#define DEFINE_BASIC_TOKEN(name, type, ...) \
  TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

#define DEFINE_COUNTER_TOKEN(name, type, ...) \
  TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)

#define DEFINE_INDEXED_TOKEN(name, type, arraysize, ...) \
  TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)

#define DEFINE_FIXED_BASIC_TOKEN(name, type, address, ...) \
  TOKEN_NEXT_ADDRESS(name, (address))                      \
  TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

#define DEFINE_FIXED_COUNTER_TOKEN(name, type, address, ...) \
  TOKEN_NEXT_ADDRESS(name, (address))                        \
  TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)

#define DEFINE_FIXED_INDEXED_TOKEN(name, type, arraysize, address, ...) \
  TOKEN_NEXT_ADDRESS(name, (address))                                   \
  TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)

#define DEFINE_MFG_TOKEN(name, type, address, ...) \
  TOKEN_NEXT_ADDRESS(name, (address))              \
  TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

// The Simulated EEPROM and NVM3 unit tests define their own tokens.
#if !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)

// The creator codes are here in one list instead of next to their token
// definitions so comparison of the codes is easier. The only requirement
// on these creator definitions is that they all must be unique. A favorite
// method for picking creator codes is to use two ASCII characters
// to make the codes more memorable.

// STACK CREATORS
#define CREATOR_STACK_NVDATA_VERSION                         0xFF01
#define CREATOR_STACK_BOOT_COUNTER                           0xE263
#define CREATOR_STACK_NONCE_COUNTER                          0xE563
#define CREATOR_STACK_ANALYSIS_REBOOT                        0xE162
#define CREATOR_STACK_KEYS                                   0xEB79
#define CREATOR_STACK_NODE_DATA                              0xEE64
#define CREATOR_STACK_CLASSIC_DATA                           0xE364
#define CREATOR_STACK_ALTERNATE_KEY                          0xE475
#define CREATOR_STACK_APS_FRAME_COUNTER                      0xE123
#define CREATOR_STACK_TRUST_CENTER                           0xE124
#define CREATOR_STACK_NETWORK_MANAGEMENT                     0xE125
#define CREATOR_STACK_PARENT_INFO                            0xE126
#define CREATOR_STACK_PARENT_ADDITIONAL_INFO                 0xE127
#define CREATOR_STACK_MULTI_PHY_NWK_INFO                     0xE128
#define CREATOR_STACK_MIN_RECEIVED_RSSI                      0xE129
// Restored EUI64
#define CREATOR_STACK_RESTORED_EUI64                         0xE12A

// MULTI-NETWORK STACK CREATORS
#define CREATOR_MULTI_NETWORK_STACK_KEYS                     0xE210
#define CREATOR_MULTI_NETWORK_STACK_NODE_DATA                0xE211
#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY            0xE212
#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER             0xE213
#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT       0xE214
#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFO              0xE215

// A temporary solution for multi-network nwk counters:
// This counter will be used on the network with index 1.
#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER            0xE220
#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO   0xE221

// GP stack tokens.
#define CREATOR_STACK_GP_DATA                                0xE258
#define CREATOR_STACK_GP_PROXY_TABLE                         0xE259
#define CREATOR_STACK_GP_SINK_TABLE                          0xE25A
#define CREATOR_STACK_GP_INCOMING_FC                         0xE25B
#define CREATOR_STACK_GP_INCOMING_FC_IN_SINK                 0xE25C
// APP CREATORS
#define CREATOR_STACK_BINDING_TABLE                          0xE274
#define CREATOR_STACK_CHILD_TABLE                            0xFF0D
#define CREATOR_STACK_KEY_TABLE                              0xE456
#define CREATOR_STACK_CERTIFICATE_TABLE                      0xE500
#define CREATOR_STACK_ZLL_DATA                               0xE501
#define CREATOR_STACK_ZLL_SECURITY                           0xE502
#define CREATOR_STACK_ADDITIONAL_CHILD_DATA                  0xE503

// NVM3KEY domain base keys
#define NVM3KEY_DOMAIN_USER    0x00000U
#define NVM3KEY_DOMAIN_ZIGBEE  0x10000U
#define NVM3KEY_DOMAIN_COMMON  0x80000U

// STACK KEYS
#define NVM3KEY_STACK_NVDATA_VERSION                       (NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
#define NVM3KEY_STACK_BOOT_COUNTER                         (NVM3KEY_DOMAIN_ZIGBEE | 0xE263)
#define NVM3KEY_STACK_NONCE_COUNTER                        (NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
#define NVM3KEY_STACK_ANALYSIS_REBOOT                      (NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
#define NVM3KEY_STACK_KEYS                                 (NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)
#define NVM3KEY_STACK_NODE_DATA                            (NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)
#define NVM3KEY_STACK_CLASSIC_DATA                         (NVM3KEY_DOMAIN_ZIGBEE | 0xE364)
#define NVM3KEY_STACK_ALTERNATE_KEY                        (NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
#define NVM3KEY_STACK_APS_FRAME_COUNTER                    (NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
#define NVM3KEY_STACK_TRUST_CENTER                         (NVM3KEY_DOMAIN_ZIGBEE | 0xE124)
#define NVM3KEY_STACK_NETWORK_MANAGEMENT                   (NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
#define NVM3KEY_STACK_PARENT_INFO                          (NVM3KEY_DOMAIN_ZIGBEE | 0xE126)
#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFO               (NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
#define NVM3KEY_STACK_MULTI_PHY_NWK_INFO                   (NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
#define NVM3KEY_STACK_MIN_RECEIVED_RSSI                    (NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
// Restored EUI64
#define NVM3KEY_STACK_RESTORED_EUI64                       (NVM3KEY_DOMAIN_ZIGBEE | 0xE12A)

// MULTI-NETWORK STACK KEYS
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_KEYS                   (NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA              (NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY          (NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER           (NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT     (NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO            (NVM3KEY_DOMAIN_ZIGBEE | 0x0280)

// Temporary solution for multi-network nwk counters:
// This counter will be used on the network with index 1.
#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER          (NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0x0300)

// GP stack tokens.
#define NVM3KEY_STACK_GP_DATA                              (NVM3KEY_DOMAIN_ZIGBEE | 0xE258)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_GP_PROXY_TABLE                       (NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_GP_SINK_TABLE                        (NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_STACK_GP_INCOMING_FC                       (NVM3KEY_DOMAIN_ZIGBEE | 0x0480)

// APP KEYS
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_BINDING_TABLE                        (NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_CHILD_TABLE                          (NVM3KEY_DOMAIN_ZIGBEE | 0x0580)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_KEY_TABLE                            (NVM3KEY_DOMAIN_ZIGBEE | 0x0600)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_CERTIFICATE_TABLE                    (NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
#define NVM3KEY_STACK_ZLL_DATA                             (NVM3KEY_DOMAIN_ZIGBEE | 0xE501)
#define NVM3KEY_STACK_ZLL_SECURITY                         (NVM3KEY_DOMAIN_ZIGBEE | 0xE502)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATA                (NVM3KEY_DOMAIN_ZIGBEE | 0x0700)

// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK               (NVM3KEY_DOMAIN_ZIGBEE | 0x0780)
// MANUFACTURING DATA
// Pull in the platform-specific manufacturing tokens
#if defined(CORTEXM3)
// Cortex-M3 handles MFG tokens separately via mfg-token.h.
#elif defined(EZSP_HOST) || defined(ZIGBEE_STACK_ON_HOST)
// No MFG tokens on hosts or Zigbeed.
#elif defined(SL_ZIGBEE_TEST)
  #include "hal/micro/unix/simulation/token-manufacturing.h"
#else
  #error no platform defined
#endif

// STACK DATA
// *The addresses of these tokens must not change.*

#define CURRENT_STACK_TOKEN_VERSION 0x03FC //MSB is version, LSB is complement.

#ifdef DEFINETYPES
typedef uint16_t tokTypeStackNvdataVersion;
typedef uint32_t tokTypeStackBootCounter;
//This was introduced to save the type of keep alives supported by the parent.
//Bits 0-2 are currently in use, bit 2 covers power negotiation.
//Bits 3-14 are reserved. Bit 15 is used in alt-mac
typedef uint16_t tokTypeStackParentAdditionalInfo;
typedef uint16_t tokTypeStackAnalysisReboot;
typedef uint32_t tokTypeStackNonceCounter;
typedef int8_t tokTypeRSSI;

// While capable series 2 parts save keys in Secure Vault, the token layout is
// left untouched. If keys have been moved to PSA, the key values in the below
// tokens are zeroed out and unused. Some tokens have bits to represent that the
// token holds an ID that points to PSA.

typedef struct {
  uint8_t networkKey[16]; // ignored if using Secure Key Storage (but moved to PSA and cleared if upgrade code is run)
  uint8_t activeKeySeqNum;
} tokTypeStackKeys;

typedef struct {
  uint16_t panId;
  int8_t radioTxPower;
  uint8_t radioFreqChannel;
  uint8_t stackProfile;
  uint8_t nodeType;
  uint16_t zigbeeNodeId;
  uint8_t extendedPanId[8];
} tokTypeStackNodeData;
typedef struct {
  uint16_t mode;
  uint8_t eui64[8];
  uint8_t key[16];  // ignored if (mode & TRUST_CENTER_KEY_LIVES_IN_PSA)
} tokTypeStackTrustCenter;
typedef struct {
  uint32_t activeChannels;
  uint16_t managerNodeId;
  uint8_t updateId;
} tokTypeStackNetworkManagement;
typedef struct {
  uint8_t parentEui[8];
  uint16_t parentNodeId;
} tokTypeStackParentInfo;
typedef struct {
  int8_t radioTxPower;
  uint8_t radioFreqChannel;
  uint32_t pg28ChannelMask;
  uint32_t pg29ChannelMask;
  uint32_t pg30ChannelMask;
  uint32_t pg31ChannelMask;
  uint8_t optionsMask;
} tokTypeStackMultiPhyNwkInfo;
typedef struct {
  uint8_t restoredEui[8];
} tokTypeStackRestoredEui64;
#endif //DEFINETYPES

#define STACK_KEYS_DEFAULT_VALUE        { { 0, } }
#define STACK_ALT_NWK_KEY_DEFAULT_VALUE { { 0, } }

#ifdef DEFINETOKENS
// The stack tokens also need to be stored at well-defined locations.
//  None of these addresses should ever change without extremely great care.
#define STACK_VERSION_LOCATION    128 //  2   bytes
#define STACK_APS_NONCE_LOCATION  130 //  4   bytes
#define STACK_ALT_NWK_KEY_LOCATION 134 // 17  bytes (key + sequence number)
// reserved                       151     1   bytes
#define STACK_BOOT_COUNT_LOCATION 152 //  2   bytes
// reserved                       154     2   bytes
#define STACK_NONCE_LOCATION      156 //  4   bytes
// reserved                       160     1   bytes
#define STACK_REBOOT_LOCATION     161 //  2   bytes
// reserved                       163     7   bytes
#define STACK_KEYS_LOCATION       170 //  17  bytes
// reserved                       187     5   bytes
#define STACK_NODE_DATA_LOCATION  192 //  16  bytes
#define STACK_CLASSIC_LOCATION    208 //  26  bytes
#define STACK_TRUST_CENTER_LOCATION 234 //26  bytes
// reserved                       260     8   bytes
#define STACK_NETWORK_MANAGEMENT_LOCATION 268 //  7   bytes
#define STACK_PARENT_INFO_LOCATION            276 //10 bytes
#define STACK_PARENT_ADDITIONAL_INFO_LOCATION 286 //2 bytes
#define STACK_MULTI_PHY_NWK_INFO_LOCATION  288    // 19 bytes
#define STACK_MIN_RECEIVED_RSSI_LOCATION    307 // 1 byte
#define STACK_RESTORED_EUI64_LOCATION       308 // 8 bytes
// reserved                       316     98 bytes

DEFINE_FIXED_BASIC_TOKEN(STACK_NVDATA_VERSION,
                         tokTypeStackNvdataVersion,
                         STACK_VERSION_LOCATION,
                         CURRENT_STACK_TOKEN_VERSION)
DEFINE_FIXED_COUNTER_TOKEN(STACK_APS_FRAME_COUNTER,
                           tokTypeStackNonceCounter,
                           STACK_APS_NONCE_LOCATION,
                           0x00000000)
DEFINE_FIXED_BASIC_TOKEN(STACK_ALTERNATE_KEY,
                         tokTypeStackKeys,
                         STACK_ALT_NWK_KEY_LOCATION,
                         STACK_ALT_NWK_KEY_DEFAULT_VALUE)
DEFINE_FIXED_COUNTER_TOKEN(STACK_BOOT_COUNTER,
                           tokTypeStackBootCounter,
                           STACK_BOOT_COUNT_LOCATION,
                           0x0000)
DEFINE_FIXED_COUNTER_TOKEN(STACK_NONCE_COUNTER,
                           tokTypeStackNonceCounter,
                           STACK_NONCE_LOCATION,
                           0x00000000)
DEFINE_FIXED_BASIC_TOKEN(STACK_ANALYSIS_REBOOT,
                         tokTypeStackAnalysisReboot,
                         STACK_REBOOT_LOCATION,
                         0x0000)
DEFINE_FIXED_BASIC_TOKEN(STACK_KEYS,
                         tokTypeStackKeys,
                         STACK_KEYS_LOCATION,
                         STACK_KEYS_DEFAULT_VALUE)
DEFINE_FIXED_BASIC_TOKEN(STACK_NODE_DATA,
                         tokTypeStackNodeData,
                         STACK_NODE_DATA_LOCATION,
                         { 0xFFFF, -1, 0, 0x00, 0x00, 0x0000 })
DEFINE_FIXED_BASIC_TOKEN(STACK_TRUST_CENTER,
                         tokTypeStackTrustCenter,
                         STACK_TRUST_CENTER_LOCATION,
                         { 0, })
DEFINE_FIXED_BASIC_TOKEN(STACK_NETWORK_MANAGEMENT,
                         tokTypeStackNetworkManagement,
                         STACK_NETWORK_MANAGEMENT_LOCATION,
                         { 0, 0xFFFF, 0 })
DEFINE_FIXED_BASIC_TOKEN(STACK_PARENT_INFO,
                         tokTypeStackParentInfo,
                         STACK_PARENT_INFO_LOCATION,
                         { { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }, 0xFFFF })
DEFINE_FIXED_BASIC_TOKEN(STACK_PARENT_ADDITIONAL_INFO,
                         tokTypeStackParentAdditionalInfo,
                         STACK_PARENT_ADDITIONAL_INFO_LOCATION,
                         0x0000)
DEFINE_FIXED_BASIC_TOKEN(STACK_MULTI_PHY_NWK_INFO,
                         tokTypeStackMultiPhyNwkInfo,
                         STACK_MULTI_PHY_NWK_INFO_LOCATION,
                         { -1, 0, 0, 0, 0, 0, 0x80 })
DEFINE_FIXED_BASIC_TOKEN(STACK_MIN_RECEIVED_RSSI,
                         tokTypeRSSI,
                         STACK_MIN_RECEIVED_RSSI_LOCATION,
                         { -100, })
DEFINE_FIXED_BASIC_TOKEN(STACK_RESTORED_EUI64,
                         tokTypeStackRestoredEui64,
                         STACK_RESTORED_EUI64_LOCATION,
                         { { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF } })
#endif //DEFINETOKENS

// PHY DATA
//
#include "token-phy.h"

// MULTI-NETWORK STACK TOKENS: Tokens for the networks with index > 0.
// The 0-index network info is stored in the usual tokens.

#ifdef DEFINETOKENS
//#if !defined(SL_ZIGBEE_MULTI_NETWORK_STRIPPED)
// SL_ZIGBEE_MULTI_NETWORK_STRIPPED is commented out to work around
// EMZIGBEE-2676 / EMHAL-1530.  This header is used somewhere
// that doesn't include sl_zigbee.h, so it leads to conflicting
// definitions. Eating the extra tokens is much easier than double
// building every library that touches a token.
#define EXTRA_NETWORKS_NUMBER (SL_ZIGBEE_SUPPORTED_NETWORKS - 1)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_KEYS,
                     tokTypeStackKeys,
                     EXTRA_NETWORKS_NUMBER,
                     STACK_KEYS_DEFAULT_VALUE)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_NODE_DATA,
                     tokTypeStackNodeData,
                     EXTRA_NETWORKS_NUMBER,
                     { 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_ALTERNATE_KEY,
                     tokTypeStackKeys,
                     EXTRA_NETWORKS_NUMBER,
                     STACK_ALT_NWK_KEY_DEFAULT_VALUE)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_TRUST_CENTER,
                     tokTypeStackTrustCenter,
                     EXTRA_NETWORKS_NUMBER,
                     { 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_NETWORK_MANAGEMENT,
                     tokTypeStackNetworkManagement,
                     EXTRA_NETWORKS_NUMBER,
                     { 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_PARENT_INFO,
                     tokTypeStackParentInfo,
                     EXTRA_NETWORKS_NUMBER,
                     { { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }, 0xFFFF })
// Temporary solution for NWK counter token: the following is used for 1-index
// network.
DEFINE_COUNTER_TOKEN(MULTI_NETWORK_STACK_NONCE_COUNTER,
                     tokTypeStackNonceCounter,
                     0x00000000)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO,
                     tokTypeStackParentAdditionalInfo,
                     EXTRA_NETWORKS_NUMBER,
                     { 0, })
//#endif // SL_ZIGBEE_MULTI_NETWORK_STRIPPED
#endif // DEFINETOKENS

// APPLICATION DATA
// *If a fixed application token is desired, its address must be above 384.*

#ifdef DEFINETYPES
typedef uint8_t tokTypeStackBindingTable[13];
typedef uint8_t tokTypeStackChildTable[11];
typedef uint8_t tokTypeStackKeyTable[25];
#define KEY_TABLE_ENTRY_SIZE       25 // 8-byte IEEE + 16-byte Key + 1-byte info
#define KEY_ENTRY_IEEE_OFFSET       0
#define KEY_ENTRY_KEY_DATA_OFFSET   8 // first 4 bytes may point to PSA ID if data[KEY_ENTRY_INFO_OFFSET] & KEY_TABLE_ENTRY_HAS_PSA_ID
#define KEY_ENTRY_INFO_OFFSET      24

typedef uint8_t tokTypeStackAdditionalChildData;
// Certificate Table Entry
//   Certificate:    48-bytes
//   CA Public Key:  22-bytes
//   Private Key:    21-bytes
//   Flags:          1-byte
#define TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE (48 + 22 + 21 + 1)
#define TOKEN_CERTIFICATE_TABLE_ENTRY_FLAGS_INDEX (TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE - 1)
typedef uint8_t tokTypeStackCertificateTable[TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE];
#endif //DEFINETYPES

// The following application tokens are required by the stack, but are sized by
//  the application via its CONFIGURATION_HEADER, which is why they are present
//  within the application data section. Any special application-defined
//  tokens will follow.
// NOTE: changing the size of these tokens within the CONFIGURATION_HEADER
//  WILL automatically move any custom application tokens that are defined
//  in the APPLICATION_TOKEN_HEADER.
#ifdef DEFINETOKENS
// Application tokens start at location 384 and are automatically positioned.
TOKEN_NEXT_ADDRESS(APP, 384)
DEFINE_INDEXED_TOKEN(STACK_BINDING_TABLE,
                     tokTypeStackBindingTable,
                     SL_ZIGBEE_BINDING_TABLE_SIZE,
                     { 0, })
DEFINE_INDEXED_TOKEN(STACK_CHILD_TABLE,
                     tokTypeStackChildTable,
                     SL_ZIGBEE_CHILD_TABLE_SIZE,
                     { 0, })
DEFINE_INDEXED_TOKEN(STACK_KEY_TABLE,
                     tokTypeStackKeyTable,
                     SL_ZIGBEE_KEY_TABLE_SIZE,
                     { 0, })
DEFINE_INDEXED_TOKEN(STACK_CERTIFICATE_TABLE,
                     tokTypeStackCertificateTable,
                     SL_ZIGBEE_CERTIFICATE_TABLE_SIZE,
                     { 0, })
DEFINE_INDEXED_TOKEN(STACK_ADDITIONAL_CHILD_DATA,
                     tokTypeStackAdditionalChildData,
                     SL_ZIGBEE_CHILD_TABLE_SIZE,
                     { 0x0F, })
#endif //DEFINETOKENS

// These must appear before the application header so that the token
// numbering is consistent regardless of whether application tokens are
// defined.
//#if defined(SL_ZIGBEE_AF_PLUGIN_ZLL_LIBRARY) || defined(SL_ZIGBEE_TEST)
  #include "stack/zll/zll-token-config.h"
  #define ZLL_TOKENS_PRESENT
//#endif
  #if !defined(EZSP_HOST)
  #if defined(SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT) || defined(JAM_BUILT_GP_LIB) || defined(SL_ZIGBEE_TEST)
    #include "stack/include/gp-token-config.h"
    #define GP_TOKENS_PRESENT
  #endif // (SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT) || (SL_ZIGBEE_TEST)
  #endif 
  #include "stack/core/multi-pan-token-config.h"

#ifndef SL_ZIGBEE_SCRIPTED_TEST
 #if (defined(SL_CATALOG_ZIGBEE_ZCL_FRAMEWORK_CORE_PRESENT) \
  || (defined(SL_CATALOG_ZIGBEE_GREEN_POWER_ADAPTER_PRESENT)))
   #include "app/framework/util/af-token.h"
 # elif defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT)
   #include "app/framework/util/af-ncp-token.h"
 #endif
#else // SL_ZIGBEE_SCRIPTED_TEST
// Unit tests may define their own token header, like em260's unit test
 #ifdef APPLICATION_TOKEN_HEADER
  #include APPLICATION_TOKEN_HEADER
 #endif
#endif // SL_ZIGBEE_SCRIPTED_TEST

//The tokens defined below are test tokens. They are normally not used
//but are left here as a convenience so test tokens do not have to
//be recreated. If test code needs temporary, non-volatile storage,
//uncomment and alter the set below as needed.
//#define CREATOR_TT01 1
//#define CREATOR_TT02 2
//#define CREATOR_TT03 3
//#define CREATOR_TT04 4
//#define CREATOR_TT05 5
//#define CREATOR_TT06 6
//#ifdef DEFINETYPES
//typedef uint32_t tokTypeTT01;
//typedef uint32_t tokTypeTT02;
//typedef uint32_t tokTypeTT03;
//typedef uint32_t tokTypeTT04;
//typedef uint16_t tokTypeTT05;
//typedef uint16_t tokTypeTT06;
//#endif //DEFINETYPES
//#ifdef DEFINETOKENS
//#define TT01_LOCATION 1
//#define TT02_LOCATION 2
//#define TT03_LOCATION 3
//#define TT04_LOCATION 4
//#define TT05_LOCATION 5
//#define TT06_LOCATION 6
//DEFINE_FIXED_BASIC_TOKEN(TT01, tokTypeTT01, TT01_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT02, tokTypeTT02, TT02_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT03, tokTypeTT03, TT03_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT04, tokTypeTT04, TT04_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT05, tokTypeTT05, TT05_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT06, tokTypeTT06, TT06_LOCATION, 0x0000)
//#endif //DEFINETOKENS

#else // !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)

//The Simulated EEPROM and NVM3 unit tests define their tokens via the
//APPLICATION_TOKEN_HEADER macro.
#ifndef SL_ZIGBEE_SCRIPTED_TEST
 #if (defined(SL_CATALOG_ZIGBEE_ZCL_FRAMEWORK_CORE_PRESENT) \
  || (defined(SL_CATALOG_ZIGBEE_GREEN_POWER_ADAPTER_PRESENT)))
   #include "app/framework/util/af-token.h"
 # elif defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT)
   #include "app/framework/util/af-ncp-token.h"
 #endif
#else // SL_ZIGBEE_SCRIPTED_TEST
 #ifdef APPLICATION_TOKEN_HEADER
  #include APPLICATION_TOKEN_HEADER
 #endif
#endif // SL_ZIGBEE_SCRIPTED_TEST

#endif // !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)

#ifndef DEFINEADDRESSES
  #undef TOKEN_NEXT_ADDRESS
#endif

Convenience Macros#

The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. See hal/micro/token.h for a more complete explanation.

#define
DEFINE_BASIC_TOKEN (name, type, ...)
#define
DEFINE_COUNTER_TOKEN (name, type, ...)
#define
DEFINE_INDEXED_TOKEN (name, type, arraysize, ...)
#define
DEFINE_FIXED_BASIC_TOKEN (name, type, address, ...)
#define
DEFINE_FIXED_COUNTER_TOKEN (name, type, address, ...)
#define
DEFINE_FIXED_INDEXED_TOKEN (name, type, arraysize, address, ...)
#define
DEFINE_MFG_TOKEN (name, type, address, ...)

Creator Codes#

The CREATOR is used as a distinct identifier tag for the token.The CREATOR is necessary because the token name is defined differently depending on the hardware platform. Therefore, the CREATOR ensures that token definitions and data stay tagged and known. The only requirement is that each creator definition must be unique. See hal/micro/token.h for a more complete explanation.

#define
#define

NVM3 Object Keys#

The NVM3 object key is used as a distinct identifier tag for a token stored in NVM3.Every token must have a defined NVM3 object key and the object key must be unique. The object key defined must be in the following format: NVM3KEY_tokennamewhere tokenname is the name of the token without NVM3KEY_ or TOKEN_ prefix.

#define
#define
#define
#define
NVM3KEY_STACK_NVDATA_VERSION (NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
#define
NVM3KEY_STACK_BOOT_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE263)
#define
NVM3KEY_STACK_NONCE_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
#define
NVM3KEY_STACK_ANALYSIS_REBOOT (NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
#define
NVM3KEY_STACK_KEYS (NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)
#define
NVM3KEY_STACK_NODE_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)
#define
NVM3KEY_STACK_CLASSIC_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE364)
#define
NVM3KEY_STACK_ALTERNATE_KEY (NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
#define
NVM3KEY_STACK_APS_FRAME_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
#define
NVM3KEY_STACK_TRUST_CENTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE124)
#define
NVM3KEY_STACK_NETWORK_MANAGEMENT (NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
#define
NVM3KEY_STACK_PARENT_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE126)
#define
NVM3KEY_STACK_PARENT_ADDITIONAL_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
#define
NVM3KEY_STACK_MULTI_PHY_NWK_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
#define
NVM3KEY_STACK_MIN_RECEIVED_RSSI (NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
#define
NVM3KEY_STACK_RESTORED_EUI64 (NVM3KEY_DOMAIN_ZIGBEE | 0xE12A)
#define
NVM3KEY_MULTI_NETWORK_STACK_KEYS (NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
#define
NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
#define
NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY (NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
#define
NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER (NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
#define
NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT (NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
#define
NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0x0280)
#define
NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
#define
#define
NVM3KEY_STACK_GP_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE258)
#define
NVM3KEY_STACK_GP_PROXY_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
#define
NVM3KEY_STACK_GP_SINK_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
#define
NVM3KEY_STACK_GP_INCOMING_FC (NVM3KEY_DOMAIN_ZIGBEE | 0x0480)
#define
NVM3KEY_STACK_BINDING_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
#define
NVM3KEY_STACK_CHILD_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0580)
#define
NVM3KEY_STACK_KEY_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0600)
#define
NVM3KEY_STACK_CERTIFICATE_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
#define
NVM3KEY_STACK_ZLL_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE501)
#define
NVM3KEY_STACK_ZLL_SECURITY (NVM3KEY_DOMAIN_ZIGBEE | 0xE502)
#define
NVM3KEY_STACK_ADDITIONAL_CHILD_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0x0700)
#define
NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK (NVM3KEY_DOMAIN_ZIGBEE | 0x0780)

Macros#

#define
TOKEN_NEXT_ADDRESS (region, address)

By default, tokens are automatically located after the previous token.

#define

The current version number of the stack tokens. MSB is the version, LSB is a complement.

#define

Convenience Macros Documentation#

DEFINE_BASIC_TOKEN#

#define DEFINE_BASIC_TOKEN
Value:
(name, type, ...)

Definition at line 104 of file stack/config/token-stack.h

DEFINE_COUNTER_TOKEN#

#define DEFINE_COUNTER_TOKEN
Value:
(name, type, ...)

Definition at line 107 of file stack/config/token-stack.h

DEFINE_INDEXED_TOKEN#

#define DEFINE_INDEXED_TOKEN
Value:
(name, type, arraysize, ...)

Definition at line 110 of file stack/config/token-stack.h

DEFINE_FIXED_BASIC_TOKEN#

#define DEFINE_FIXED_BASIC_TOKEN
Value:
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

Definition at line 113 of file stack/config/token-stack.h

DEFINE_FIXED_COUNTER_TOKEN#

#define DEFINE_FIXED_COUNTER_TOKEN
Value:
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)

Definition at line 117 of file stack/config/token-stack.h

DEFINE_FIXED_INDEXED_TOKEN#

#define DEFINE_FIXED_INDEXED_TOKEN
Value:
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)

Definition at line 121 of file stack/config/token-stack.h

DEFINE_MFG_TOKEN#

#define DEFINE_MFG_TOKEN
Value:
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

Definition at line 125 of file stack/config/token-stack.h

Creator Codes Documentation#

CREATOR_STACK_NVDATA_VERSION#

#define CREATOR_STACK_NVDATA_VERSION
Value:
0xFF01

Definition at line 154 of file stack/config/token-stack.h

CREATOR_STACK_BOOT_COUNTER#

#define CREATOR_STACK_BOOT_COUNTER
Value:
0xE263

Definition at line 155 of file stack/config/token-stack.h

CREATOR_STACK_NONCE_COUNTER#

#define CREATOR_STACK_NONCE_COUNTER
Value:
0xE563

Definition at line 156 of file stack/config/token-stack.h

CREATOR_STACK_ANALYSIS_REBOOT#

#define CREATOR_STACK_ANALYSIS_REBOOT
Value:
0xE162

Definition at line 157 of file stack/config/token-stack.h

CREATOR_STACK_KEYS#

#define CREATOR_STACK_KEYS
Value:
0xEB79

Definition at line 158 of file stack/config/token-stack.h

CREATOR_STACK_NODE_DATA#

#define CREATOR_STACK_NODE_DATA
Value:
0xEE64

Definition at line 159 of file stack/config/token-stack.h

CREATOR_STACK_CLASSIC_DATA#

#define CREATOR_STACK_CLASSIC_DATA
Value:
0xE364

Definition at line 160 of file stack/config/token-stack.h

CREATOR_STACK_ALTERNATE_KEY#

#define CREATOR_STACK_ALTERNATE_KEY
Value:
0xE475

Definition at line 161 of file stack/config/token-stack.h

CREATOR_STACK_APS_FRAME_COUNTER#

#define CREATOR_STACK_APS_FRAME_COUNTER
Value:
0xE123

Definition at line 162 of file stack/config/token-stack.h

CREATOR_STACK_TRUST_CENTER#

#define CREATOR_STACK_TRUST_CENTER
Value:
0xE124

Definition at line 163 of file stack/config/token-stack.h

CREATOR_STACK_NETWORK_MANAGEMENT#

#define CREATOR_STACK_NETWORK_MANAGEMENT
Value:
0xE125

Definition at line 164 of file stack/config/token-stack.h

CREATOR_STACK_PARENT_INFO#

#define CREATOR_STACK_PARENT_INFO
Value:
0xE126

Definition at line 165 of file stack/config/token-stack.h

CREATOR_STACK_PARENT_ADDITIONAL_INFO#

#define CREATOR_STACK_PARENT_ADDITIONAL_INFO
Value:
0xE127

Definition at line 166 of file stack/config/token-stack.h

CREATOR_STACK_MULTI_PHY_NWK_INFO#

#define CREATOR_STACK_MULTI_PHY_NWK_INFO
Value:
0xE128

Definition at line 167 of file stack/config/token-stack.h

CREATOR_STACK_MIN_RECEIVED_RSSI#

#define CREATOR_STACK_MIN_RECEIVED_RSSI
Value:
0xE129

Definition at line 168 of file stack/config/token-stack.h

CREATOR_STACK_RESTORED_EUI64#

#define CREATOR_STACK_RESTORED_EUI64
Value:
0xE12A

Definition at line 170 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_KEYS#

#define CREATOR_MULTI_NETWORK_STACK_KEYS
Value:
0xE210

Definition at line 173 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_NODE_DATA#

#define CREATOR_MULTI_NETWORK_STACK_NODE_DATA
Value:
0xE211

Definition at line 174 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY#

#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY
Value:
0xE212

Definition at line 175 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER#

#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER
Value:
0xE213

Definition at line 176 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#

#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT
Value:
0xE214

Definition at line 177 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_PARENT_INFO#

#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFO
Value:
0xE215

Definition at line 178 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER#

#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER
Value:
0xE220

Definition at line 182 of file stack/config/token-stack.h

CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#

#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO
Value:
0xE221

Definition at line 183 of file stack/config/token-stack.h

CREATOR_STACK_GP_DATA#

#define CREATOR_STACK_GP_DATA
Value:
0xE258

Definition at line 186 of file stack/config/token-stack.h

CREATOR_STACK_GP_PROXY_TABLE#

#define CREATOR_STACK_GP_PROXY_TABLE
Value:
0xE259

Definition at line 187 of file stack/config/token-stack.h

CREATOR_STACK_GP_SINK_TABLE#

#define CREATOR_STACK_GP_SINK_TABLE
Value:
0xE25A

Definition at line 188 of file stack/config/token-stack.h

CREATOR_STACK_GP_INCOMING_FC#

#define CREATOR_STACK_GP_INCOMING_FC
Value:
0xE25B

Definition at line 189 of file stack/config/token-stack.h

CREATOR_STACK_GP_INCOMING_FC_IN_SINK#

#define CREATOR_STACK_GP_INCOMING_FC_IN_SINK
Value:
0xE25C

Definition at line 190 of file stack/config/token-stack.h

CREATOR_STACK_BINDING_TABLE#

#define CREATOR_STACK_BINDING_TABLE
Value:
0xE274

Definition at line 192 of file stack/config/token-stack.h

CREATOR_STACK_CHILD_TABLE#

#define CREATOR_STACK_CHILD_TABLE
Value:
0xFF0D

Definition at line 193 of file stack/config/token-stack.h

CREATOR_STACK_KEY_TABLE#

#define CREATOR_STACK_KEY_TABLE
Value:
0xE456

Definition at line 194 of file stack/config/token-stack.h

CREATOR_STACK_CERTIFICATE_TABLE#

#define CREATOR_STACK_CERTIFICATE_TABLE
Value:
0xE500

Definition at line 195 of file stack/config/token-stack.h

CREATOR_STACK_ZLL_DATA#

#define CREATOR_STACK_ZLL_DATA
Value:
0xE501

Definition at line 196 of file stack/config/token-stack.h

CREATOR_STACK_ZLL_SECURITY#

#define CREATOR_STACK_ZLL_SECURITY
Value:
0xE502

Definition at line 197 of file stack/config/token-stack.h

CREATOR_STACK_ADDITIONAL_CHILD_DATA#

#define CREATOR_STACK_ADDITIONAL_CHILD_DATA
Value:
0xE503

Definition at line 198 of file stack/config/token-stack.h

NVM3 Object Keys Documentation#

NVM3KEY_DOMAIN_USER#

#define NVM3KEY_DOMAIN_USER
Value:
0x00000U

Definition at line 219 of file stack/config/token-stack.h

NVM3KEY_DOMAIN_ZIGBEE#

#define NVM3KEY_DOMAIN_ZIGBEE
Value:
0x10000U

Definition at line 220 of file stack/config/token-stack.h

NVM3KEY_DOMAIN_COMMON#

#define NVM3KEY_DOMAIN_COMMON
Value:
0x80000U

Definition at line 221 of file stack/config/token-stack.h

NVM3KEY_STACK_NVDATA_VERSION#

#define NVM3KEY_STACK_NVDATA_VERSION
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)

Definition at line 224 of file stack/config/token-stack.h

NVM3KEY_STACK_BOOT_COUNTER#

#define NVM3KEY_STACK_BOOT_COUNTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE263)

Definition at line 225 of file stack/config/token-stack.h

NVM3KEY_STACK_NONCE_COUNTER#

#define NVM3KEY_STACK_NONCE_COUNTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE563)

Definition at line 226 of file stack/config/token-stack.h

NVM3KEY_STACK_ANALYSIS_REBOOT#

#define NVM3KEY_STACK_ANALYSIS_REBOOT
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE162)

Definition at line 227 of file stack/config/token-stack.h

NVM3KEY_STACK_KEYS#

#define NVM3KEY_STACK_KEYS
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)

Definition at line 228 of file stack/config/token-stack.h

NVM3KEY_STACK_NODE_DATA#

#define NVM3KEY_STACK_NODE_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)

Definition at line 229 of file stack/config/token-stack.h

NVM3KEY_STACK_CLASSIC_DATA#

#define NVM3KEY_STACK_CLASSIC_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE364)

Definition at line 230 of file stack/config/token-stack.h

NVM3KEY_STACK_ALTERNATE_KEY#

#define NVM3KEY_STACK_ALTERNATE_KEY
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE475)

Definition at line 231 of file stack/config/token-stack.h

NVM3KEY_STACK_APS_FRAME_COUNTER#

#define NVM3KEY_STACK_APS_FRAME_COUNTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE123)

Definition at line 232 of file stack/config/token-stack.h

NVM3KEY_STACK_TRUST_CENTER#

#define NVM3KEY_STACK_TRUST_CENTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE124)

Definition at line 233 of file stack/config/token-stack.h

NVM3KEY_STACK_NETWORK_MANAGEMENT#

#define NVM3KEY_STACK_NETWORK_MANAGEMENT
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE125)

Definition at line 234 of file stack/config/token-stack.h

NVM3KEY_STACK_PARENT_INFO#

#define NVM3KEY_STACK_PARENT_INFO
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE126)

Definition at line 235 of file stack/config/token-stack.h

NVM3KEY_STACK_PARENT_ADDITIONAL_INFO#

#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFO
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE127)

Definition at line 236 of file stack/config/token-stack.h

NVM3KEY_STACK_MULTI_PHY_NWK_INFO#

#define NVM3KEY_STACK_MULTI_PHY_NWK_INFO
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE128)

Definition at line 237 of file stack/config/token-stack.h

NVM3KEY_STACK_MIN_RECEIVED_RSSI#

#define NVM3KEY_STACK_MIN_RECEIVED_RSSI
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE129)

Definition at line 238 of file stack/config/token-stack.h

NVM3KEY_STACK_RESTORED_EUI64#

#define NVM3KEY_STACK_RESTORED_EUI64
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE12A)

Definition at line 240 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_KEYS#

#define NVM3KEY_MULTI_NETWORK_STACK_KEYS
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0000)

Definition at line 244 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA#

#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0080)

Definition at line 246 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY#

#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0100)

Definition at line 248 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER#

#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0180)

Definition at line 250 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#

#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0200)

Definition at line 252 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO#

#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0280)

Definition at line 254 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER#

#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE220)

Definition at line 258 of file stack/config/token-stack.h

NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#

#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0300)

Definition at line 260 of file stack/config/token-stack.h

NVM3KEY_STACK_GP_DATA#

#define NVM3KEY_STACK_GP_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE258)

Definition at line 263 of file stack/config/token-stack.h

NVM3KEY_STACK_GP_PROXY_TABLE#

#define NVM3KEY_STACK_GP_PROXY_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0380)

Definition at line 265 of file stack/config/token-stack.h

NVM3KEY_STACK_GP_SINK_TABLE#

#define NVM3KEY_STACK_GP_SINK_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0400)

Definition at line 267 of file stack/config/token-stack.h

NVM3KEY_STACK_GP_INCOMING_FC#

#define NVM3KEY_STACK_GP_INCOMING_FC
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0480)

Definition at line 269 of file stack/config/token-stack.h

NVM3KEY_STACK_BINDING_TABLE#

#define NVM3KEY_STACK_BINDING_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0500)

Definition at line 273 of file stack/config/token-stack.h

NVM3KEY_STACK_CHILD_TABLE#

#define NVM3KEY_STACK_CHILD_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0580)

Definition at line 275 of file stack/config/token-stack.h

NVM3KEY_STACK_KEY_TABLE#

#define NVM3KEY_STACK_KEY_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0600)

Definition at line 277 of file stack/config/token-stack.h

NVM3KEY_STACK_CERTIFICATE_TABLE#

#define NVM3KEY_STACK_CERTIFICATE_TABLE
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0680)

Definition at line 279 of file stack/config/token-stack.h

NVM3KEY_STACK_ZLL_DATA#

#define NVM3KEY_STACK_ZLL_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE501)

Definition at line 280 of file stack/config/token-stack.h

NVM3KEY_STACK_ZLL_SECURITY#

#define NVM3KEY_STACK_ZLL_SECURITY
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE502)

Definition at line 281 of file stack/config/token-stack.h

NVM3KEY_STACK_ADDITIONAL_CHILD_DATA#

#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATA
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0700)

Definition at line 283 of file stack/config/token-stack.h

NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK#

#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK
Value:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0780)

Definition at line 286 of file stack/config/token-stack.h

Macro Definition Documentation#

TOKEN_NEXT_ADDRESS#

#define TOKEN_NEXT_ADDRESS

By default, tokens are automatically located after the previous token.

If a token needs to be placed at a specific location, one of the DEFINE_FIXED_* definitions should be used. This macro is inherently used in the DEFINE_FIXED_* definition to locate a token and under special circumstances (such as manufacturing tokens) it may be explicitly used.


Definition at line 69 of file stack/config/token-stack.h

CURRENT_STACK_TOKEN_VERSION#

#define CURRENT_STACK_TOKEN_VERSION
Value:
0x03FC

The current version number of the stack tokens. MSB is the version, LSB is a complement.

See hal/micro/token.h for a more complete explanation.


Definition at line 312 of file stack/config/token-stack.h

STACK_KEYS_DEFAULT_VALUE#

#define STACK_KEYS_DEFAULT_VALUE
Value:
{ { 0, } }

Definition at line 372 of file stack/config/token-stack.h

STACK_ALT_NWK_KEY_DEFAULT_VALUE#

#define STACK_ALT_NWK_KEY_DEFAULT_VALUE
Value:
{ { 0, } }

Definition at line 373 of file stack/config/token-stack.h

ZLL_TOKENS_PRESENT#

#define ZLL_TOKENS_PRESENT

Definition at line 578 of file stack/config/token-stack.h