Public Attributes#

ZW_APPLICATION_TX_BUFFER *
uint8_t
uint8_t

Public Attribute Documentation#

frame#

ZW_APPLICATION_TX_BUFFER* _cc_handler_output_t::frame

Definition at line 204 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

length#

uint8_t _cc_handler_output_t::length

Definition at line 205 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

duration#

uint8_t _cc_handler_output_t::duration

Definition at line 206 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h