EventDistributor object.

All content is private.

Public Attributes#

uint8_t

Number of entries in pEventHandlerTable.

pointer to const array of Callback function pointers - Event handlers

void(*

Callback to handler of Notification with no event and wait for event timeout

Public Attribute Documentation#

iEventHandlerTableSize#

uint8_t SEventDistributor::iEventHandlerTableSize

Number of entries in pEventHandlerTable.


Definition at line 78 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Components/EventDistributor/EventDistributor.h

pEventHandlerTable#

const EventDistributorEventHandler* SEventDistributor::pEventHandlerTable

pointer to const array of Callback function pointers - Event handlers


Definition at line 79 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Components/EventDistributor/EventDistributor.h

pNoEvent#

void(* SEventDistributor::pNoEvent) (void)

Callback to handler of Notification with no event and wait for event timeout


Definition at line 81 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Components/EventDistributor/EventDistributor.h