Public Attribute Documentation#
sof#
uint8_t tx_beam_stop_frame_t::sof
Definition at line
106
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
type#
uint8_t tx_beam_stop_frame_t::type
Definition at line
107
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp1#
uint8_t tx_beam_stop_frame_t::timestamp1
Definition at line
108
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp2#
uint8_t tx_beam_stop_frame_t::timestamp2
Definition at line
109
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
rssi#
uint8_t tx_beam_stop_frame_t::rssi
Definition at line
110
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
counter#
uint16_t tx_beam_stop_frame_t::counter
Definition at line
111
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h