Zpal-retention-register#

Defines a platform abstraction layer for the Z-Wave retention register.

How to use the retention register API

The retention register should support at least 32 x 32 bit registers which can be retained in deep sleep.

The following outlines an example of use:

  1. Store value in retention register using zpal_retention_register_write().

  2. Read value from retention register using zpal_retention_register_read().

Note:

  • Retention registers with index 0-15 are reserved for Z-Wave protocol code.

  • Retention registers are frequently written, so it is not recommended to use flash memory as storage.

Functions#

zpal_retention_register_read(uint32_t index, uint32_t *data)

Reads a 32-bit value from the specified retention register.

zpal_retention_register_write(uint32_t index, uint32_t value)

Write a 32-bit value to the specified retention register.

size_t

Get number of available retention registers.

Function Documentation#

zpal_retention_register_read#

zpal_status_t zpal_retention_register_read (uint32_t index, uint32_t * data)

Reads a 32-bit value from the specified retention register.

Parameters
[in]index

Retention register number (zero-based).

[out]data

Pointer to a 32-bit variable where the value can be stored.

Returns

Note

  • Retention Register should support at least 32 objects.


Definition at line 62 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

zpal_retention_register_write#

zpal_status_t zpal_retention_register_write (uint32_t index, uint32_t value)

Write a 32-bit value to the specified retention register.

Parameters
[in]index

Retention register number (zero-based).

[in]value

32-bit value to save in retention register.

Returns

Note

  • Retention Register should support at least 32 objects.


Definition at line 74 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

zpal_retention_register_count#

size_t zpal_retention_register_count (void )

Get number of available retention registers.

Parameters
N/A

Returns

  • number of retention registers.


Definition at line 80 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

Macro Definition Documentation#

ZPAL_RETENTION_REGISTER_SMARTSTART#

#define ZPAL_RETENTION_REGISTER_SMARTSTART
Value:
0

Definition at line 43 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_RESPONSEROUTE_1#

#define ZPAL_RETENTION_REGISTER_RESPONSEROUTE_1
Value:
1

Definition at line 44 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_RESPONSEROUTE_2#

#define ZPAL_RETENTION_REGISTER_RESPONSEROUTE_2
Value:
2

Definition at line 45 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_RESPONSEROUTE_3#

#define ZPAL_RETENTION_REGISTER_RESPONSEROUTE_3
Value:
3

Definition at line 46 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_RESPONSEROUTE_4#

#define ZPAL_RETENTION_REGISTER_RESPONSEROUTE_4
Value:
4

Definition at line 47 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_TXPOWER_RSSI_LR#

#define ZPAL_RETENTION_REGISTER_TXPOWER_RSSI_LR
Value:
5

Definition at line 48 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h

ZPAL_RETENTION_REGISTER_PROTOCOL_RESERVED_COUNT#

#define ZPAL_RETENTION_REGISTER_PROTOCOL_RESERVED_COUNT
Value:
16

Definition at line 50 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_retention_register.h