Z-Wave Serial API#
Modules#
Enumerations#
enum
FIRMWARE_UPDATE_NVM_INIT = 0
FIRMWARE_UPDATE_NVM_SET_NEW_IMAGE = 1
FIRMWARE_UPDATE_NVM_GET_NEW_IMAGE = 2
FIRMWARE_UPDATE_NVM_UPDATE_CRC16 = 3
FIRMWARE_UPDATE_NVM_IS_VALID_CRC16 = 4
FIRMWARE_UPDATE_NVM_WRITE = 5
FIRMWARE_UPDATE_NVM_UNKNOWN = 0xFF
}
Firmware update functionality specifics Enum definitions for Firmware Update functionality selector; firmwareUpdateFunction.
Macros#
#define
SOF 0x01
Start Of Frame.
#define
ACK 0x06
Acknowledge successful frame reception.
#define
NAK 0x15
Not Acknowledge successful frame reception - please retransmit...
#define
CAN 0x18
Frame received (from host) was dropped - waiting for ACK.
Enumeration Documentation#
FIRMWARE_UPDATE_NVM_T#
FIRMWARE_UPDATE_NVM_T
Firmware update functionality specifics Enum definitions for Firmware Update functionality selector; firmwareUpdateFunction.
Enumerator | |
---|---|
FIRMWARE_UPDATE_NVM_INIT | |
FIRMWARE_UPDATE_NVM_SET_NEW_IMAGE | |
FIRMWARE_UPDATE_NVM_GET_NEW_IMAGE | |
FIRMWARE_UPDATE_NVM_UPDATE_CRC16 | |
FIRMWARE_UPDATE_NVM_IS_VALID_CRC16 | |
FIRMWARE_UPDATE_NVM_WRITE | |
FIRMWARE_UPDATE_NVM_UNKNOWN |
Definition at line
41
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h
Macro Definition Documentation#
SOF#
#define SOFValue:
0x01
Start Of Frame.
Definition at line
16
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h
ACK#
#define ACKValue:
0x06
Acknowledge successful frame reception.
Definition at line
17
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h
NAK#
#define NAKValue:
0x15
Not Acknowledge successful frame reception - please retransmit...
Definition at line
18
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h
CAN#
#define CANValue:
0x18
Frame received (from host) was dropped - waiting for ACK.
Definition at line
19
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h