ZAF Event Handling#
Functions#
void
ZAF_JobHelperInit(void)
Initializes the job helper.
bool
ZAF_JobHelperJobEnqueue(uint8_t event)
Adds a given event to the job queue.
bool
ZAF_JobHelperJobDequeue(uint8_t *pEvent)
Dequeues a job from the job queue.
uint8_t
Returns the current number of jobs on the job queue.
Macros#
#define
Defines the maximum number of jobs to queue for this module.
Function Documentation#
ZAF_JobHelperInit#
void ZAF_JobHelperInit (void )
Initializes the job helper.
Parameters
N/A |
Definition at line
27
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_job_helper.h
ZAF_JobHelperJobEnqueue#
bool ZAF_JobHelperJobEnqueue (uint8_t event)
Adds a given event to the job queue.
Parameters
[in] | event | An event. |
Returns
true if the event was added to the job queue, false otherwise.
Definition at line
34
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_job_helper.h
ZAF_JobHelperJobDequeue#
bool ZAF_JobHelperJobDequeue (uint8_t * pEvent)
Dequeues a job from the job queue.
Parameters
[out] | pEvent | return event from the queue. |
Returns
true if a job was dequeued, false otherwise.
Definition at line
41
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_job_helper.h
ZAF_JobHelperGetNumberOfRemainingJobs#
uint8_t ZAF_JobHelperGetNumberOfRemainingJobs (void )
Returns the current number of jobs on the job queue.
Parameters
N/A |
Returns
Number of jobs on the job queue.
Definition at line
47
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_job_helper.h