Defines all data related to the Configuration CC.

Public Attribute Documentation#

numberOfParameters#

uint16_t cc_configuration_t::numberOfParameters

Definition at line 124 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h

parameters#

const cc_config_parameter_metadata_t* cc_configuration_t::parameters

Definition at line 125 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h