Door Lock Capabilities Report data structure.#
This allows the Application to inform the Command Class handler of the capabilities of the Door Lock.
The supportedOperationTypeBitmask field indicates the Supported Operations Modes:
Bit 0 in Bit Mask 1: Reserved
Bit 1 in Bit Mask 1: Constant Operation
Bit 2 in Bit Mask 1: Timed Operation.
The supportedDoorLockModeList indicates the Supported Door Lock Modes:
0x00: Door Unsecured
0x01: Door unsecured with timeout
0x10: Door Unsecured for Inside Door Handles
0x11: Door Unsecured for Inside Door Handles with timeout
0x20: Door Unsecured for Outside Door Handles
0x21: Door Unsecured for Outside Door Handles with timeout
0xFF: Door Secured
Inside/outside Door Handles Modes supported These mode bits indicate which handles are supported on the Door Lock.
The mode of the four inside and four outside door handles are encoded in supportedInsideHandleModes and supportedOutsideHandleModes as:
Bit 0: Handle 1
Bit 1: Handle 2
Bit 2: Handle 3
Bit 3: Handle 4 Values:
0: disabled
1: enabled
Supported Door Components. The supportedDoorComponents field indicates the supported Door Lock components: such as bolt and latch states.
Bit 0: Door
Bit 1: Bolt
Bit 2: Latch
Bit 3-7: Reserved
Auto Relock Support The autoRelockSupport flag indicates if the Door Lock Supports Auto Relock (1=supported, 0=not supported).
Hold And Release Support The holdAndReleaseSupport flag indicates if the Door Lock Supports * Hold And Releaese (1=supported, 0=not supported),
Twist Assist Support The twistAssistSupport flag indicates if the Door Lock Supports Twist Assist (1=supported, 0=not supported),
Block To Block Support The blockToBlockSupport flag indicates if the Door Lock Supports Block To Block (1=supported, 0=not supported),
Public Attributes#
Reserved (2 bits)
Length of Supported Operation Type Bitmask (5 bits)
Supported Operation Types.
Length of supported Door Lock Mode List.
List of Supported Door Lock Modes.
Supported Outside Handle Modes bitmask (4 bits)
Supported Inside Handle Modes bitmask (4 bits)
Supported Door Components.
Indicates if the lock supports Auto Relock.
Indicates if the lock supports Hold And Release.
Indicates if the lock supports Twist Assist.
Indicates if the lock supports Twist Assist.
Public Attribute Documentation#
reserved#
uint8_t cc_door_lock_capabilities_report_t::reserved
Reserved (2 bits)
145
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
lengthSupportedOperationType#
uint8_t cc_door_lock_capabilities_report_t::lengthSupportedOperationType
Length of Supported Operation Type Bitmask (5 bits)
146
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
supportedOperationTypeBitmask#
uint8_t cc_door_lock_capabilities_report_t::supportedOperationTypeBitmask
Supported Operation Types.
Max. length fixed to 1 byte. Enough to hold both defined types defined in SDS13781.
147
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
lengthSupportedDoorLockModeList#
uint8_t cc_door_lock_capabilities_report_t::lengthSupportedDoorLockModeList
Length of supported Door Lock Mode List.
148
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
supportedDoorLockModeList#
uint8_t cc_door_lock_capabilities_report_t::supportedDoorLockModeList[8]
List of Supported Door Lock Modes.
Max. Length fixed to 8 byte. Enough to hold all modes defined in SDS13781.
149
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
supportedOutsideHandleModes#
uint8_t cc_door_lock_capabilities_report_t::supportedOutsideHandleModes
Supported Outside Handle Modes bitmask (4 bits)
150
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
supportedInsideHandleModes#
uint8_t cc_door_lock_capabilities_report_t::supportedInsideHandleModes
Supported Inside Handle Modes bitmask (4 bits)
151
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
supportedDoorComponents#
uint8_t cc_door_lock_capabilities_report_t::supportedDoorComponents
Supported Door Components.
152
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
autoRelockSupport#
uint8_t cc_door_lock_capabilities_report_t::autoRelockSupport
Indicates if the lock supports Auto Relock.
153
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
holdAndReleaseSupport#
uint8_t cc_door_lock_capabilities_report_t::holdAndReleaseSupport
Indicates if the lock supports Hold And Release.
154
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
twistAssistSupport#
uint8_t cc_door_lock_capabilities_report_t::twistAssistSupport
Indicates if the lock supports Twist Assist.
155
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h
blockToBlockSupport#
uint8_t cc_door_lock_capabilities_report_t::blockToBlockSupport
Indicates if the lock supports Twist Assist.
156
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/DoorLock/inc/CC_DoorLock.h