Public Attributes#

const void *

This must point to a global data.

uint8_t

Public Attribute Documentation#

data#

const void* event_cc_t::data

This must point to a global data.


Definition at line 23 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_event_distributor_soc.h

command_class#

uint16_t event_cc_t::command_class

Definition at line 24 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_event_distributor_soc.h

event#

uint8_t event_cc_t::event

Definition at line 25 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/EventHandling/zaf_event_distributor_soc.h