Network Learn Mode#
Functions#
void
ZAF_setNetworkLearnMode(E_NETWORK_LEARN_MODE_ACTION bMode)
Sets network learn mode to given value.
Function Documentation#
ZAF_setNetworkLearnMode#
void ZAF_setNetworkLearnMode (E_NETWORK_LEARN_MODE_ACTION bMode)
Sets network learn mode to given value.
Parameters
N/A | bMode | Network mode to be set. Refer to E_NETWORK_LEARN_MODE_ACTION |
This function is called when node should be added or removed from the network, or to enable Smart Start.
Definition at line
29
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_network_learn.h