Security Keys Bitmask#

Bitmask for security keys.

Macro Definition Documentation#

SECURITY_KEY_S2_UNAUTHENTICATED_BIT#

#define SECURITY_KEY_S2_UNAUTHENTICATED_BIT
Value:
0x01

Definition at line 38 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h

SECURITY_KEY_S2_AUTHENTICATED_BIT#

#define SECURITY_KEY_S2_AUTHENTICATED_BIT
Value:
0x02

Definition at line 39 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h

SECURITY_KEY_S2_ACCESS_BIT#

#define SECURITY_KEY_S2_ACCESS_BIT
Value:
0x04

Definition at line 40 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h

SECURITY_KEY_S0_BIT#

#define SECURITY_KEY_S0_BIT
Value:
0x80

Definition at line 41 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h

SECURITY_KEY_S2_MASK#

#define SECURITY_KEY_S2_MASK
Value:
(SECURITY_KEY_S2_UNAUTHENTICATED_BIT \
| SECURITY_KEY_S2_AUTHENTICATED_BIT \
| SECURITY_KEY_S2_ACCESS_BIT)

Definition at line 43 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h

SECURITY_KEY_NONE_MASK#

#define SECURITY_KEY_NONE_MASK
Value:
0x00

Definition at line 46 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_security_api.h