ZAF_Transport_Multicast#
Enumerations#
Functions#
Initiates transmission of a frame and will handle multi channel and multicast transmissions.
Initializes the Tx Buffer.
Enumeration Documentation#
ETRANSPORT_MULTICAST_STATUS#
ETRANSPORT_MULTICAST_STATUS
Enumerator | |
---|---|
ETRANSPORTMULTICAST_FAILED | |
ETRANSPORTMULTICAST_ADDED_TO_QUEUE |
22
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportMulticast.h
Function Documentation#
ZW_TransportMulticast_SendRequest#
enum ETRANSPORT_MULTICAST_STATUS ZW_TransportMulticast_SendRequest (const uint8_t *const p_data, uint8_t data_length, uint8_t fSupervisionEnable, TRANSMIT_OPTIONS_TYPE_EX * p_nodelist, ZAF_TX_Callback_t p_callback)
Initiates transmission of a frame and will handle multi channel and multicast transmissions.
[in] | p_data | Pointer to data. |
[in] | data_length | Length of data in bytes. |
[in] | fSupervisionEnable | Enable Supervision encapsulation if set to true. |
[in] | p_nodelist | Pointer to a list of nodes. |
[in] | p_callback | Pointer to a callback function which is called for each transmission to a node. |
If the node has associations to multiple endpoints of the same node, this function will transmit one multi channel encapsulated frame that addresses the associated endpoints.
If the node is included using S2 and has more than one non-endpoint association, this function will transmit an S2 multicast (broadcast) frame addressing those associations followed by singlecast follow-up frames.
If the node is included using S0 there will be no multicast since S0 does not support multicast.
If the node is non-securely included and has more than one non-endpoint association, this function will transmit a non-secure multicast followed by singlecast follow-up frames.
Returns
Returns status of transmission.
51
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportMulticast.h
ZW_TransportMulticast_clearTimeout#
void ZW_TransportMulticast_clearTimeout (void )
N/A |
60
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportMulticast.h
ZW_TransportMulticast_init#
void ZW_TransportMulticast_init (void )
Initializes the Tx Buffer.
N/A |
66
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportMulticast.h