Zpal-nvm#
Defines a platform abstraction layer for the Z-Wave NVM.
How to use the entropy API
The ZPAL NVM provides a way for an application to safely store and retrieve variable size data in a page-based non-volatile memory (NVM). Data are identified with 20-bit identifiers denoted as data_id.
The following outlines an example of use:
Initialize module with zpal_nvm_init().
Invoke zpal_nvm_write() to store data.
Invoke zpal_nvm_read() to get data.
Enumerations#
Defines the different areas of NVM storage.
Functions#
Initializes the NVM for a given area.
Closes the NVM of a given handle.
Reads object from a given area handle and given object key.
Reads part of object from a given area handle and given object key.
Writes object to a given area handle and given object key.
Erases everything in a given area.
Delete an object from NVM.
Get the object size identified with a given key from NVM.
Create a list of key for valid objects in NVM.
Opens the NVM for a backup/restore operation.
Closes the NVM after backup/restore operation.
Reads raw data from the NVM.
Writes raw data to the NVM.
Get size of raw NVM area.
Set write protection for storage.
Migrates 800s legacy application file system to shared app/protocol file system.
Enumeration Documentation#
zpal_nvm_area_t#
zpal_nvm_area_t
Defines the different areas of NVM storage.
Enumerator | |
---|---|
ZPAL_NVM_AREA_APPLICATION | Reserved for application data. |
ZPAL_NVM_AREA_ZAF | Reserved for ZAF data. |
ZPAL_NVM_AREA_STACK | Reserved for stack data. |
ZPAL_NVM_AREA_MANUFACTURER_TOKENS | Reserved for manufacturer tokens. |
45
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
Typedef Documentation#
zpal_nvm_object_key_t#
typedef uint32_t zpal_nvm_object_key_t
Data id type.
Only the 20 least significant bits are used.
56
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_handle_t#
typedef void* zpal_nvm_handle_t
Defines the NVM handle type.
61
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
Function Documentation#
zpal_nvm_init#
zpal_nvm_handle_t zpal_nvm_init (zpal_nvm_area_t area)
Initializes the NVM for a given area.
[in] | area | NVM area to initialize. |
Returns
A valid NVM handle if successfully initialized. Otherwise it returns NULL.
69
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_close#
zpal_status_t zpal_nvm_close (zpal_nvm_handle_t handle)
Closes the NVM of a given handle.
[in] | handle | NVM area handle. |
Returns
ZPAL_STATUS_OK if the file system was successfully closed and ZPAL_STATUS_FAIL otherwise.
77
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_read#
zpal_status_t zpal_nvm_read (zpal_nvm_handle_t handle, zpal_nvm_object_key_t key, void * object, size_t object_size)
Reads object from a given area handle and given object key.
[in] | handle | NVM area handle. |
[in] | key | Object key. |
[out] | object | Address of array where object can be written to. |
[in] | object_size | Size of the stored object. |
Returns
ZPAL_STATUS_OK if the object was successfully read and ZPAL_STATUS_FAIL otherwise.
88
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_read_object_part#
zpal_status_t zpal_nvm_read_object_part (zpal_nvm_handle_t handle, zpal_nvm_object_key_t key, void * object, size_t offset, size_t object_size)
Reads part of object from a given area handle and given object key.
[in] | handle | NVM area handle. |
[in] | key | Object key. |
[out] | object | Address of array where object can be written to. |
[in] | offset | The offset where object shall be read from. |
[in] | object_size | Size of the stored object. |
Returns
ZPAL_STATUS_OK if the object was successfully read and ZPAL_STATUS_FAIL otherwise.
100
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_write#
zpal_status_t zpal_nvm_write (zpal_nvm_handle_t handle, zpal_nvm_object_key_t key, const void * object, size_t object_size)
Writes object to a given area handle and given object key.
[in] | handle | NVM area handle. |
[in] | key | Object key. |
[out] | object | Address of array of object that must be written. |
[in] | object_size | Size of the object to be stored. |
Returns
ZPAL_STATUS_OK if the object was successfully written and ZPAL_STATUS_FAIL otherwise.
111
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_erase_all#
zpal_status_t zpal_nvm_erase_all (zpal_nvm_handle_t handle)
Erases everything in a given area.
[in] | handle | NVM area handle. |
Returns
ZPAL_STATUS_OK if the all objects was successfully erased and ZPAL_STATUS_FAIL otherwise.
119
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_erase_object#
zpal_status_t zpal_nvm_erase_object (zpal_nvm_handle_t handle, zpal_nvm_object_key_t key)
Delete an object from NVM.
[in] | handle | Nvm storage handle. |
[in] | key | Object key. |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
128
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_get_object_size#
zpal_status_t zpal_nvm_get_object_size (zpal_nvm_handle_t handle, zpal_nvm_object_key_t key, size_t * len)
Get the object size identified with a given key from NVM.
[in] | handle | Nvm storage handle. |
[in] | key | Object key. |
[out] | len | Object size. |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
138
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_enum_objects#
size_t zpal_nvm_enum_objects (zpal_nvm_handle_t handle, zpal_nvm_object_key_t * key_list, size_t key_list_size, zpal_nvm_object_key_t key_min, zpal_nvm_object_key_t key_max)
Create a list of key for valid objects in NVM.
[in] | handle | Nvm storage handle. |
[out] | key_list | A pointer to a buffer for the key list. |
[in] | key_list_size | The size of the key list buffer. |
[in] | key_min | The lower search key. |
[in] | key_max | The upper search key. |
Returns
The number of keys written to the key list. This value is less than or equal to
key_list_size
.
150
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_backup_open#
zpal_status_t zpal_nvm_backup_open (void )
Opens the NVM for a backup/restore operation.
N/A |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
161
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_backup_close#
void zpal_nvm_backup_close (void )
Closes the NVM after backup/restore operation.
N/A |
166
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_backup_read#
zpal_status_t zpal_nvm_backup_read (uint32_t offset, void * data, size_t data_length)
Reads raw data from the NVM.
[in] | offset | The offset where data shall be read from. |
[out] | data | Address of array where data can be written to. |
[in] | data_length | Length of the stored data. |
Returns
ZPAL_STATUS_OK if the data was successfully read and ZPAL_STATUS_FAIL otherwise.
176
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_backup_write#
zpal_status_t zpal_nvm_backup_write (uint32_t offset, const void * data, size_t data_length)
Writes raw data to the NVM.
[in] | offset | The offset where data shall be written to. |
[out] | data | Address of array of data that must be written. |
[in] | data_length | Length of the data to be stored. |
Returns
ZPAL_STATUS_OK if the data was successfully written and ZPAL_STATUS_FAIL otherwise.
186
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_backup_get_size#
size_t zpal_nvm_backup_get_size (void )
Get size of raw NVM area.
N/A |
Returns
Size of raw NVM area.
193
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_lock#
zpal_status_t zpal_nvm_lock (zpal_nvm_handle_t handle)
Set write protection for storage.
[in] | handle | Nvm storage handle. |
Returns
ZPAL_STATUS_OK if the lock was set successfully, ZPAL_STATUS_FAIL otherwise.
201
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h
zpal_nvm_migrate_legacy_app_file_system#
zpal_status_t zpal_nvm_migrate_legacy_app_file_system (void )
Migrates 800s legacy application file system to shared app/protocol file system.
N/A |
Returns
ZPAL_STATUS_OK if the file system was successfully migrated and ZPAL_STATUS_FAIL otherwise.
208
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_nvm.h